This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a few questions about DLPC3479's adderss.
In the DLPC3479 Software Programmer's Guide, DLPC3479's I2C slave address is descrived as "0x36 (0x3A)".
Which device use 0x3A? And if I send the I2C command to 0x3A, Can I get same response as 0x36 ?
Regards,
Goto.
Hi Keisuke,
Welcome to TI E2E Forums! The DLPC3479 will respond only on 0x36 and not on 0x3A. Usage of the address 0x3A instead of the default 0x36 address requires specially modified FW from TI.
Hi Hirak,
Thank you for your response.
>Usage of the address 0x3A instead of the default 0x36 address requires specially modified FW from TI.
I've understood. Can I also use the address other thant 0x36 and 0x3A if modified FW by TI ?
Regards,
Goto
Hi Goto,
The controller supports only the following 2 I2C addresses -0x36 and 0x3A
Regards,
Mayank