Hi,
my question refers to another thread posted before: "DLPC350: 8bit pattern sequence result makes border".
I am observing the same behavior. I am using the LCR4500 EVM with cameras for structured light measurement tasks.
As seen in the image below, there is a visible "edge" in the middle of the image. The image is taken by a camera which is triggered by the projector. Exposure times are matched.
For the usual measurement I am using sine patterns with different frequencies and those "artifacts" are affecting the overall measurement quality. In case of the sine patterns, the "edges" are located at the turning point of the sine wave.
My thoughts so far:
- This effect seems to occur at the middle of the displayable color depth - ~127 for 8-bit uint.
- It may be caused by the PWM of the DMD? - I played with the image exposure time and was able to catch the first division of illuminated and not illuminated regions. The edge seems to occur on the border of those regions.
Any thoughts or suggestions on how to approach this?