Other Parts Discussed in Thread: TMS320VC5501
Hello great people,
Im a newbee just entering the DSP world.
Im trying to create custom board with TMS320VC5501 DSP, had some research and got to know that DSP gets booted from external slow NV-memory as oppose to microcontroller which have onchip flash memory. So I'hv chosen to interface serial flash thruogh MCBSP0 using SPI protocol with appropriate boot mode.
I also know JTAG is used for debugging purposes supporting hardware breakpoints in CCS.
My concern is how to program external EEPROM which is @ MCBSP0 port of DSP.
Is there any way that I can program EEPROM through JTAG?, Not sure how does Flashburn/SDFlash works !
There is some help available on http://processors.wiki.ti.com/index.php/SPI_Boot_on_5502_EVM
but it dosen't says how does <Burning the Image to SPI Flash | option 3> works
Thanks in advance