This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320VC5501 SPI EEPROM Boot Mode

Other Parts Discussed in Thread: TMS320VC5501, TMS320C2834X

Hello great people,

Im a newbee just entering the DSP world.

Im trying to create custom board with TMS320VC5501 DSP, had some research and got to know that DSP gets booted from external slow NV-memory as oppose to microcontroller which have onchip flash memory.  So I'hv chosen to interface serial flash thruogh MCBSP0 using SPI protocol with appropriate boot mode.

I also know JTAG is used for debugging purposes supporting hardware breakpoints in CCS.

My concern is how to program external EEPROM which is @ MCBSP0 port of DSP.

Is there any way that I can program EEPROM through JTAG?, Not sure how does Flashburn/SDFlash works !

 

There is some help available on http://processors.wiki.ti.com/index.php/SPI_Boot_on_5502_EVM

but it dosen't says how does <Burning the Image to SPI Flash | option 3>  works

 

Thanks in advance