Other Parts Discussed in Thread: TCI6636K2H
Hello,
we are planning a design based on a 66AK2H6 with a HyperLink connection to a FPGA under high data bandwidth requirements (~15 Gbit/s in each direction) for wireless communication.
From our knowledge the EVMK2HX evaluation module is currently not available in Europe. Please correct me, if I am wrong. As we want to start the software development and evaluation as soon as possible, we are thinking of using a similar Keystone I platform like the TMDXEVM6678L in a first step. And when the 66AK2H6 comes available, we are planning to switch over. The hardware board development will be done from the beginning for the 66AK2H6.
So far I read several user guides, white papers and datasheets for the Keystone I and II.
Therefore I have got several questions:
- Do you know when the EVMK2HX comes available in Europe?
- How easy is it to switch from the C667x to the 66AK2H6 in terms of software reusability?
Are all the libraries/ interfaces (e.g. Hyperlink, IPC, DSPLib, Multicore programming..) of the SYS/BIOS and LINUX-MCSDK for both platforms the same? Which are the points we have to be aware of in our development? I have seen that the MCSDK 03_00_00_11 only supports the new Keystone II platforms for example. - So far I understand that the Keystone II architecture is pretty similar to the Keystone I, but increases the data backbone performance between the cores significantly. And it adds ARM cores as well as more I/O capabilities. Is there something else we have to be aware of, when changing platforms?
- Is there already a throughput performance guide like for the C66x Keystone I devices available? Can I assume that the Keystone II devices reach at least the Keystone I numbers?
- Is there data available for the performance of a FFT with 2048 points on a single C66x K2 DSP core (not the FFTC!)? We are interested in the calculation time.
- We are also interested in using the TCI6636K2H instead. As information about this SoC is pretty rare, can you provide us a release date for this chip? It has really nice Coprocessors.
- Is there any data available for a 25 Gbit/s HyperLink throughput performance between a TMDXEVM6678L and a Xilinx Kintex-7 FPGA with the Integretek IP-HyperLink with a 0,5m HyperLink connection cable? Is it possible to reach the 15 Gbit/s in both directions?
Thanks in advance for your time!
Best regards