This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buid error in adding NDK to existing project



Hi,

I am just adding NDK to existing project.

In project proerty, I checked NDK and checked to add NDK/Global to my configuration.

I got the following build error:

undefined first referenced
symbol in file
--------- ----------------
NIMUDeviceTable C:\ti\ndk_2_21_02_43\packages\ti\ndk\stack\lib\stk6.ae66<nimu.oe66>

error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "nara_dsp_platform.out" not built

what library do I need to add?

I am in a hurry and need your prompt support.

Thanks in advance.

Baeyoung

  • Your log seems to be you haven't used NIMU driver in your project.
    C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\debug\ti.transport.ndk.nimu.ae66

    Do you have the following line in your *.cfg ?

    var NdkTransport = xdc.loadPackage('ti.transport.ndk');
  • Dear Titus,

    I appreciate your help.

    Do you mean that I just need to add "NdkTranport" to *.cfg?

    or also do I need to ti.transport.ndk.nimu.ae66 library to "include library file" of file search path in projet property?

    When I added one line to *.cfg, I got another error like the following,

     undefined                   first referenced                                                                                          
      symbol                         in file                                                                                               
     ---------                   ----------------                                                                                          
     Cppi_configureRxFlow        C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Osal_cppiCsEnter            C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Osal_cppiCsExit             C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Osal_nimuFree               C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Osal_nimuMalloc             C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Osal_qmssCsEnter            C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Osal_qmssCsExit             C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Pa_addMac                   C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Pa_forwardResult            C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     QMSS_QPOP                   C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     QMSS_QPUSH                  C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     QMSS_QPUSHDESCSIZE          C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_ackInterrupt           C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_disableAccumulator     C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_getQueueNumber         C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_programAccumulator     C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_queueClose             C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_queueOpen              C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     Qmss_setEoiVector           C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     qmssLObj                    C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     res_mgr_cppi_get_passhandle C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     res_mgr_get_painstance      C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     res_mgr_qmss_get_freeq      C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     res_mgr_stop_cppi           C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>
     res_mgr_stop_qmss           C:\ti\pdk_C6678_1_1_2_6\packages\ti\transport\ndk\nimu\lib\release\ti.transport.ndk.nimu.ae66<nimu_eth.obj>

    error #10234-D: unresolved symbols remain

    error #10010: errors encountered during linking; "nara_dsp_platform.out" not built
    >> Compilation failure

    I'm afraid to say that I need your prompt help for this issue.

    I'm attaching my c file and cfg file for your help.

    /*
     *  ======== main.c ========
     */
    
    #include <xdc/std.h>
    
    #include <xdc/runtime/Error.h>
    #include <xdc/runtime/System.h>
    
    #include <ti/sysbios/BIOS.h>
    
    #include <ti/sysbios/knl/Task.h>
    
    // added ByPark
    #include <ctype.h>
    #include <ti/ndk/inc/netmain.h>
    #include <xdc/runtime/Memory.h>
    #include <ti/sysbios/family/c64p/Hwi.h>
    #include <ti/sysbios/knl/Swi.h>
    #include <ti/sysbios/family/c66/tci66xx/CpIntc.h>
    #include <ti/csl/csl_gpio.h>
    #include <ti/csl/csl_gpioAux.h>
    /* NIMU */
    #include "ti/transport/ndk/nimu/nimu_eth.h"
    #include "ti\platform\platform.h"
    #include "ti\platform\resource_mgr.h"
    #include "ti/csl/cslr_uart.h"
    #include "ti\platform\evmc6678l\platform_lib\include\evmc66x_uart.h"
    #include "ti\platform\evmc6678l\platform_lib\include\evmc66x_gpio.h"
    //#define CSL_UART_REGS 0x02540000
    #define hUartRegs ((CSL_UartRegs*)	CSL_UART_REGS)
    #define GPIO_CFG_BASE				(0x02320000)
    #define GPIO_REG_BINTEN				(0x8)
    #define GPIO_REG_DIR				(0x10)
    #define GPIO_REG_OUT_DATA			(0x14)
    #define GPIO_REG_SET_DATA			(0x18)
    #define GPIO_REG_CLR_DATA			(0x1C)
    #define GPIO_REG_IN_DATA			(0x20)
    #define GPIO_REG_SET_RIS_TRIG		(0x24)
    #define GPIO_REG_CLR_RIS_TRIG		(0x28)
    #define GPIO_REG_SET_FAL_TRIG		(0x2C)
    #define GPIO_REG_CLR_FAL_TRIG		(0x30)
    
    #define NOR_DEVICE					PLATFORM_DEVID_NORN25Q128;
    
    unsigned int GPIO_INT_DONE = 0;
    
    Void HWI_UART_Handler(UArg arg);
    Void HWI_GPIO_Handler(UArg arg);
    void SWI_UART_Handler();
    void SWI_GPIO_Handler();
    void UART_Idle_Handler();
    void SPI_NOR_Read(/*int length*/);
    
    extern Swi_Handle uartSwiHandle;
    extern Swi_Handle gpioSwiHandle;
    
    unsigned int Uart_Interrupt_Received_Flag = 0;
    static char cmdString[30];
    static unsigned int cmdStringPtr = NULL;
    
    /* OSAL functions for Platform Library */
    uint8_t *Osal_platformMalloc (uint32_t num_bytes, uint32_t alignment)
    {
    	return malloc(num_bytes);
    }
    
    void Osal_platformFree (uint8_t *dataPtr, uint32_t num_bytes)
    {
    	/* Free up the memory */
    	if (dataPtr)
    	{
    		free(dataPtr);
    	}
    }
    
    void Osal_platformSpiCsEnter(void)
    {
    	/* Get the hardware semaphore.
    	 *
    	 * Acquire Multi core CPPI synchronization lock
    	 */
    	while ((CSL_semAcquireDirect (PLATFORM_SPI_HW_SEM)) == 0)
    		;
    	return;
    }
    
    void Osal_platformSpiCsExit (void)
    {
    	/* Release the hardware semaphore
    	 *
    	 * Release multi-core lock.
    	 */
    	CSL_semReleaseSemaphore (PLATFORM_SPI_HW_SEM);
    	return;
    }
    
    /*
     *  ======== taskFxn ========
     */
    //Void taskFxn(UArg a0, UArg a1)
    //{
    //    System_printf("enter taskFxn()\n");
    //
    //    Task_sleep(10);
    //
    //    System_printf("exit taskFxn()\n");
    //}
    
    /*
     *  ======== main ========
     */
    Void main()
    { 
    	int i=0;
    
        System_printf("enter main()\n");
    
    	// enable ERBI & ELSI of IER for UART
        CSL_FINS (hUartRegs->IER, UART_IER_ERBI,  CSL_UART_IER_ERBI_ENABLE);
        CSL_FINS (hUartRegs->IER, UART_IER_ELSI,  CSL_UART_IER_ELSI_ENABLE);
        // mapping system interrupt(148) to host interrupt(32)
        CpIntc_mapSysIntToHostInt(0,148,32);
        CpIntc_dispatchPlug(148, &HWI_UART_Handler,0, TRUE);
        CpIntc_enableHostInt(0,32);
        CpIntc_clearSysInt(0,148);
    
        //set GPIO_0 pin as an input
        *(unsigned int*)(GPIO_CFG_BASE+GPIO_REG_DIR) |= 0x1;
        //set falling edge to trigger GPIO_0 interrupt
        *(unsigned int*)(GPIO_CFG_BASE+GPIO_REG_SET_FAL_TRIG) |= 0x1;
        //clear rising edge trigger of GPIO_0 interrupt
        *(unsigned int*)(GPIO_CFG_BASE+GPIO_REG_SET_RIS_TRIG) &= 0xFFFFFFFE;
        //enable GPIO interrupts
        *(unsigned int*)(GPIO_CFG_BASE+GPIO_REG_BINTEN) |= 0x1;
    
        for(i=0;i<4;i++)
    		platform_led(i, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
    
        platform_write("\nStart BIOS 6\n");
    	platform_write("NARA DSP Platform Started.\n");
    
    	memset(cmdString, 0, /*sizeof(memset)*/30);
    	cmdStringPtr = NULL;
    
        BIOS_start();     /* enable interrupts and start SYS/BIOS */
    }
    
    /*************************************************************************
    * EVM_init()
    * Initializes the platform hardware. This routine is configured to start in
    * the evm.cfg configuration file. It is the first routine that BIOS
    * calls and is executed before Main is called. If you are debugging within
    * CCS the default option in your target configuration file may be to execute
    * all code up until Main as the image loads. To debug this you should disable
    * that option.
    ************************************************************************/
    void EVM_init()
    {
    	platform_init_flags sFlags;
    	platform_init_config sConfig;
    	int32_t pform_status;
    	/* Initialize the UART */
    	platform_uart_init();
    	platform_uart_set_baudrate(115200);
    	(void) platform_write_configure(PLATFORM_WRITE_ALL);
    	/*
    	* You can choose what to initialize on the platform by setting the following
    	* flags. Things like the DDR, PLL, etc should have been set by the boot loader.
    	*/
    	memset( (void *) &sFlags, 0, sizeof(platform_init_flags));
    	memset( (void *) &sConfig, 0, sizeof(platform_init_config));
    	sFlags.pll = 0;		/* PLLs for clocking */
    	sFlags.ddr = 0;		/* External memory */
    	sFlags.tcsl = 1;	/* Time stamp counter */
    	sFlags.phy = 0;		/* Ethernet */
    	sFlags.ecc = 0;		/* Memory ECC */
    	sConfig.pllm = 0;	/* Use libraries default clock divisor */
    	pform_status = platform_init(&sFlags, &sConfig);
    	/* If we initialized the platform okay */
    	if (pform_status != Platform_EOK)
    	{
    		/* Initialization of the platform failed... die */
    		platform_write("Platform failed to initialize. Error code %d \n", pform_status);
    		platform_write("We will die in an infinite loop... \n");
    		while (1)
    		{
    			(void) platform_led(1, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
    			(void) platform_delay(50000);
    			(void) platform_led(1, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
    			(void) platform_delay(50000);
    		}
    	}
    
    	return;
    }
    
    Void HWI_UART_Handler(UArg arg)
    {
    //	static int LED0_state = 0;
    //	uint8_t UART_Byte_Recv;
    
    	Swi_post(uartSwiHandle);
    
    //	CpIntc_clearSysInt(0,148);
    //	UART_Byte_Recv=UartReadData();
    //	if(LED0_state)
    //		platform_led(0, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
    //	else
    //		platform_led(0, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
    //	LED0_state ^= 1;
    }
    
    Void HWI_GPIO_Handler(UArg arg)
    {
    	Swi_post(gpioSwiHandle);
    }
    
    void SWI_UART_Handler()
    {
    	static int LED0_state = 0;
    
    	Uart_Interrupt_Received_Flag = 1;
    
    	CpIntc_clearSysInt(0,148);
    
    	if(LED0_state)
    		platform_led(0, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
    	else
    		platform_led(0, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
    	LED0_state ^= 1;
    }
    
    void SWI_GPIO_Handler()
    {
    	static int LED2_state = 0;
    
    	Uart_Interrupt_Received_Flag = 2;
    
    	if(LED2_state)
    		platform_led(2, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
    	else
    		platform_led(2, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
    	LED2_state ^= 1;
    }
    
    void CLK_LED_Handler(void)
    {
    	static int LED1_state = 0;
    
    	if(LED1_state)
    		platform_led(1, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
    	else
    		platform_led(1, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
    
    	LED1_state ^= 1;
    }
    
    void UART_Idle_Handler()
    {
    	uint8_t UART_Byte_Recv;
    	unsigned int indata;
    
    	switch(Uart_Interrupt_Received_Flag)
    	{
    	case 1:
    		Uart_Interrupt_Received_Flag = 0;
    		UART_Byte_Recv=UartReadData();
    		if(UART_Byte_Recv==0xD) {
    			platform_uart_write(0xA);
    			platform_uart_write(UART_Byte_Recv);
    
    			if(strncmp("NOR read", cmdString, 8)==0) {
    
    				SPI_NOR_Read();
    				platform_uart_write(0xA);	// LF
    				platform_uart_write(0xD);	// CR
    			}
    
    			memset(cmdString, 0, /*sizeof(memset)*/30);
    			cmdStringPtr = 0;
    		}
    		else {
    			platform_uart_write(UART_Byte_Recv);
    			cmdString[cmdStringPtr++] = UART_Byte_Recv;
    		}
    		break;
    	case 2:
    		Uart_Interrupt_Received_Flag = 0;
    		// read GPIO_0 status
    		indata = gpioReadInput(GPIO_0);
    		if(indata)
    			platform_write("\nGPIO(0) high\n");
    		else
    			platform_write("\nGPIO(0) low\n");
    		break;
    	default:
    		break;
    	}
    }
    
    void SPI_NOR_Read(/*int length*/)
    {
    	int32_t					block, page;
    	uint32_t				deviceid;
    //	uint32_t				flash_selection = NULL;
    	uint32_t				offset;
    	uint8_t					*buffer = NULL;
    	PLATFORM_DEVICE_info	*p_device = NULL;
    	Error_Block				errorBlock;
    	int						i;
    
    	deviceid = NOR_DEVICE;
    
    	p_device = platform_device_open(deviceid, 0);
    	if(p_device==NULL) {
    		platform_write("\nUnable to open NOR Flash\n");
    		goto READ_DONE;
    	}
    
    	buffer = (uint8_t *) Memory_alloc( NULL, platform_roundup(p_device->page_size, PLATFORM_CACHE_LINE_SIZE), PLATFORM_CACHE_LINE_SIZE, &errorBlock);
    	if(!buffer) {
    		platform_write("Unable to allocate memory to read NOR flash\n");
    		goto READ_DONE;
    	}
    
    	memset(buffer, 0, p_device->page_size);
    	block = 0;
    	page = 0;
    
    	platform_blocknpage_to_offset(p_device->handle, &offset, block, page);
    
    	platform_device_read(p_device->handle, offset, buffer, p_device->page_size);
    
    	for(i=0;i<128;i++)
    	{
    		platform_write("%02X", buffer[i]);
    	}
    
    READ_DONE:
    	if(buffer)
    		Memory_free(NULL, buffer, platform_roundup(p_device->page_size, PLATFORM_CACHE_LINE_SIZE));
    
    	if(p_device!=NULL)
    		platform_device_close(p_device->handle);
    
    	return;
    }
    

    nara_dsp.cfg

    Thanks in advance.

    Baeyoung

  • Dear Titus,
    Thanks for your help.
    I compared my *.cfg with *.cfg of helloWord. And I found I need more package including cppi, qmss and pa.
    I finally cleared my build error.
    Thanks so much.
    Bye
  • Sounds good.
    Actually just now I am looking into those *.cfg files for comparison.
    Glad to hear.
    Thanks for your update.