Other Parts Discussed in Thread: SYSBIOS
Hello again.
Still the same board (TMDSEVM6670L), still the same problems.
I want to send from the PC (client) the string array to the board (server) and send back the string array, which is declared on board. I use this code on PC (client):
SOCKET mysocket;
if (INVALID_SOCKET == (mysocket = socket (AF_INET, SOCK_STREAM, 0) ) )
{
// Error...
error = WSAGetLastError();
// ...
}
sockaddr_in mysocket_addr;
ZeroMemory (&mysocket_addr, sizeof (mysocket_addr));
mysocket_addr.sin_family = AF_INET;
mysocket_addr.sin_addr.S_un.S_addr = inet_addr ("192.168.1.200");
mysocket_addr.sin_port = htons (1234);
if (SOCKET_ERROR == ( connect (mysocket, (sockaddr *) &mysocket_addr, sizeof (mysocket_addr) ) ) )
{
// Error...
error = WSAGetLastError();
// ...
}
if (SOCKET_ERROR == ( send (mysocket, sHELLO, sizeof(sHELLO), 0 ) ) )
{
// Error...
error = WSAGetLastError();
// ...
}
if (SOCKET_ERROR == ( recv (mysocket, (char* ) & buff, sizeof(*buff), 0 ) ) )
{
// Error...
error = WSAGetLastError();
// ...
}
closesocket(mysocket);
And this code on server (board):
SOCKET s;
SOCKET client_socket;
struct sockaddr_in server_addr;
server_addr.sin_family = AF_INET;
server_addr.sin_port = htons(1234);
server_addr.sin_addr.s_addr = inet_addr("192.168.1.200");
s = socket (AF_INET, SOCK_STREAM, 0);
bind(s, (struct sockaddr*)& server_addr, sizeof(server_addr));
struct sockaddr_in client_addr;
client_addr.sin_addr.s_addr = inet_addr("192.168.1.1");
int client_addr_size=sizeof(client_addr);
client_socket=accept(s, (struct sockaddr *)&client_addr, &client_addr_size);
//connect - bind - accept - send - recieve
listen(s, 0x100);
for (;;)
{
recv(client_socket,&buff[0],sizeof(buff),0);
send(client_socket,message,sizeof(message),0);
}
Still i'm thinking that i've done everything completely wrong, so i;m really asking for help. And also, can i use not the "7" port for the connection, because it's using only for testing?
And also... I must use "sendto" and "recvfrom", or simple "send" and "recieve" would be enough?