Dear all,
We are working on a C6654 platform that has a DDR3 clock is synchronized at 1333 MHz. The chip is a micron one 16 Meg x 16 x 8 banks.
The input clock is at 66.67MHz. We load the image using a bootloader firmware that download the final image using PCIe, as in the examples that are provided in the mcsdk_2_01_02_06 .
For configre the PLL and DDR3 we used the code that is provided by TI under pdk6657 folder and we have modified this to be align with the clock specification for the C6654 clock.
When the program starts the DDR3 is initialized and stable. But when we access a specific region of memory and initialized some addresses with the value -1 , 0xFFFF_FFFF hex we noticed that some values of this section periodically changes one specific bit from 1 to 0.
It is the same bit for all the address, the 16bit in the sequence.
For instance instead of 0xFFFF_FFFF we have 0xFFFD_FFFF. The program is halted and no interrupts runs in the system at the time that the values changes.
We have already run a program that test the DDR3 and no error has occurred when read/write from and to DDR3.
Could please give us any hint what probably goes wrong?
//NOTE: code that we use for the DDR3 initialization, provided by TI without any change
CSL_Status DDR3Init()
{
CSL_Status status = CSL_SOK;
volatile unsigned int loopCount;
uint32_t ddr3config, ddrPhyCtrl;
uint8_t ddrPHYReadLatency;
EMIF4F_TIMING1_CONFIG sdram_tim1;
EMIF4F_TIMING2_CONFIG sdram_tim2;
EMIF4F_TIMING3_CONFIG sdram_tim3;
EMIF4F_OUTPUT_IMP_CONFIG zqcfg;
EMIF4F_PWR_MGMT_CONFIG pwrmgmtcfg;
EMIF4F_SDRAM_CONFIG sdramcfg;
CSL_BootCfgUnlockKicker();
/* Wait for PLL to lock = min 500 ref clock cycles.
With refclk = 100MHz, = 5000 ns = 5us */
platform_delaycycles(50000);
/**************** 3.3 Leveling Register Configuration ********************/
CSL_BootCfgGetDDRConfig(0, &ddr3config);
ddr3config &= ~(0x007FE000); // clear ctrl_slave_ratio field
CSL_BootCfgSetDDRConfig(0, ddr3config);
CSL_BootCfgGetDDRConfig(0, &ddr3config);
ddr3config |= 0x00200000; // set ctrl_slave_ratio to 0x100
CSL_BootCfgSetDDRConfig(0, ddr3config);
CSL_BootCfgGetDDRConfig(12, &ddr3config);
ddr3config |= 0x08000000; // Set invert_clkout = 1
CSL_BootCfgSetDDRConfig(12, ddr3config);
CSL_BootCfgGetDDRConfig(0, &ddr3config);
ddr3config |= 0xF; // set dll_lock_diff to 15
CSL_BootCfgSetDDRConfig(0, ddr3config);
CSL_BootCfgGetDDRConfig(23, &ddr3config);
ddr3config |= 0x00000200; // See section 4.2.1, set for partial automatic levelling
CSL_BootCfgSetDDRConfig(23, ddr3config);
/**************** 3.3 Partial Automatic Leveling ********************/
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(2, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(3, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(4, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(5, ddr3config);
ddr3config = 0x00000033; CSL_BootCfgSetDDRConfig(6, ddr3config);
ddr3config = 0x0000003A; CSL_BootCfgSetDDRConfig(7, ddr3config);
ddr3config = 0x0000002C; CSL_BootCfgSetDDRConfig(8, ddr3config);
ddr3config = 0x0000002C; CSL_BootCfgSetDDRConfig(9, ddr3config);
ddr3config = 0x0000001C; CSL_BootCfgSetDDRConfig(10, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(14, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(15, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(16, ddr3config);
ddr3config = 0x00; CSL_BootCfgSetDDRConfig(17, ddr3config);
ddr3config = 0x000000B7; CSL_BootCfgSetDDRConfig(18, ddr3config);
ddr3config = 0x000000B1; CSL_BootCfgSetDDRConfig(19, ddr3config);
ddr3config = 0x000000A4; CSL_BootCfgSetDDRConfig(20, ddr3config);
ddr3config = 0x000000A4; CSL_BootCfgSetDDRConfig(21, ddr3config);
ddr3config = 0x00000098; CSL_BootCfgSetDDRConfig(22, ddr3config);
/*Do a PHY reset. Toggle DDR_PHY_CTRL_1 bit 15 0->1->0 */
CSL_EMIF4F_GetPhyControl(&ddrPhyCtrl, &ddrPHYReadLatency);
ddrPhyCtrl &= ~(0x00008000);
CSL_EMIF4F_SetPhyControl(ddrPhyCtrl, ddrPHYReadLatency);
CSL_EMIF4F_GetPhyControl(&ddrPhyCtrl, &ddrPHYReadLatency);
ddrPhyCtrl |= (0x00008000);
CSL_EMIF4F_SetPhyControl(ddrPhyCtrl, ddrPHYReadLatency);
CSL_EMIF4F_GetPhyControl(&ddrPhyCtrl, &ddrPHYReadLatency);
ddrPhyCtrl &= ~(0x00008000);
CSL_EMIF4F_SetPhyControl(ddrPhyCtrl, ddrPHYReadLatency);
/***************** 3.4 Basic Controller and DRAM configuration ************/
/* enable configuration */
/* hEmif->SDRAM_REF_CTRL = 0x00006180; */
CSL_EMIF4F_EnableInitRefresh();
CSL_EMIF4F_SetRefreshRate(0x515C);
sdram_tim1.t_wtr = 4;
sdram_tim1.t_rrd = 1;
sdram_tim1.t_rc = 0x20;
sdram_tim1.t_ras = 0x17;
sdram_tim1.t_wr = 0x09;
sdram_tim1.t_rcd = 0x09;
sdram_tim1.t_rp = 0x09;
CSL_EMIF4F_SetTiming1Config(&sdram_tim1);
/* hEmif->SDRAM_TIM_2 = 0x40877FEC; */
sdram_tim2.t_cke = 3;
sdram_tim2.t_rtp = 4;
sdram_tim2.t_xsrd = 0x1FF;
sdram_tim2.t_xsnr = 0x071;
sdram_tim2.t_xp = 3;
sdram_tim2.t_odt = 0;
CSL_EMIF4F_SetTiming2Config (&sdram_tim2);
/* hEmif->SDRAM_TIM_3 = 0x55BF87FF; */
sdram_tim3.t_rasMax = 0xF;
sdram_tim3.t_rfc = 0x06A;
sdram_tim3.t_tdqsckmax = 0;
sdram_tim3.zq_zqcs = 0x3F;
sdram_tim3.t_ckesr = 4;
sdram_tim3.t_csta = 0x5;
sdram_tim3.t_pdll_ul = 0x5;
CSL_EMIF4F_SetTiming3Config (&sdram_tim3);
/* hEmif->DDR_PHY_CTRL_1 = 0x0010010F; */
ddrPHYReadLatency = 0x0F;
ddrPhyCtrl = (0x0010010F);
CSL_EMIF4F_SetPhyControl(ddrPhyCtrl, ddrPHYReadLatency);
/* hEmif->ZQ_CONFIG = 0x70074C1F; */
zqcfg.zqRefInterval = 0x4C1F;
zqcfg.zqZQCLMult = 3;
zqcfg.zqZQCLInterval = 1;
zqcfg.zqSFEXITEn = 1;
zqcfg.zqDualCSEn = 1;
zqcfg.zqCS0En = 1;
zqcfg.zqCS1En = 0;
CSL_EMIF4F_SetOutputImpedanceConfig(&zqcfg);
/* hEmif->PWR_MGMT_CTRL = 0x0; */
pwrmgmtcfg.csTime = 0;
pwrmgmtcfg.srTime = 0;
pwrmgmtcfg.lpMode = 0;
pwrmgmtcfg.dpdEnable = 0;
pwrmgmtcfg.pdTime = 0;
CSL_EMIF4F_SetPowerMgmtConfig (&pwrmgmtcfg);
/* New value with DYN_ODT disabled and SDRAM_DRIVE = RZQ/7 */
/* hEmif->SDRAM_CONFIG = 0x63077AB3; */
CSL_EMIF4F_GetSDRAMConfig (&sdramcfg);
#if defined CHIP_6657
sdramcfg.pageSize = 2;
# elif defined CHIP_6654
//NOTE:check this again
sdramcfg.pageSize = 2;
# else
#error MKSTR(__FILE__) MKSTR(__LINE__)
# endif
sdramcfg.eBank = 0;
sdramcfg.iBank = 3;
sdramcfg.rowSize = 5;
sdramcfg.CASLatency = 14;
sdramcfg.narrowMode = 1;
# if defined CHIP_6657
sdramcfg.CASWriteLat = 0;
# elif defined CHIP_6654
sdramcfg.CASWriteLat = 3;
# else
#error MKSTR(__FILE__) MKSTR(__LINE__)
# endif
sdramcfg.SDRAMDrive = 1;
sdramcfg.disableDLL = 0;
sdramcfg.dynODT = 2;
sdramcfg.ddrDDQS = 0;
sdramcfg.ddrTerm = 2;
sdramcfg.iBankPos = 0;
sdramcfg.type = 3;
CSL_EMIF4F_SetSDRAMConfig (&sdramcfg);
cycles_delay(840336); /*Wait 600us for HW init to complete*/
/* Refresh rate = (7.8*666MHz] */
/* hEmif->SDRAM_REF_CTRL = 0x00001450; */
CSL_EMIF4F_SetRefreshRate(0x0000144F);
/***************** 4.2.1 Partial automatic leveling ************/
/* hEmif->RDWR_LVL_RMP_CTRL = 0x80000000; */
CSL_EMIF4F_SetLevelingRampControlInfo(1, 0, 0, 0, 0);
/* Trigger full leveling - This ignores read DQS leveling result and uses ratio forced value */
/* hEmif->RDWR_LVL_CTRL = 0x80000000; */
CSL_EMIF4F_SetLevelingControlInfo(1, 0, 0, 0, 0);
/************************************************************
Wait for min 1048576 DDR clock cycles for leveling to complete
= 1048576 * 1.5ns = 1572864ns = 1.57ms.
Actual time = ~10-15 ms
**************************************************************/
cycles_delay(4201680); //Wait 3ms for leveling to complete
return (status);
}
/******************************************************************************************** * Platform Specific Declarations * *******************************************************************************************/ #define PLATFORM_INFO_CPU_NAME "TMS320C6657" #define PLATFORM_INFO_BOARD_NAME "TMDXEVM6657L" #define MEGM_REV_ID_REGISTER (0x01812000) #define MEGM_REV_ID_MAJ_MASK (0xFFFF0000) #define MEGM_REV_ID_MAJ_SHIFT (16) #define MEGM_REV_ID_MIN_MASK (0x0000FFFF) #define MEGM_REV_ID_MIN_SHIFT (0) #define CSL_MDIO_0_REGS (CSL_EMAC_SS_CFG_REGS + 0x0800) /* Clock rate */ # if defined CHIP_6657 #define PLATFORM_BASE_CLK_RATE_MHZ (67) # elif defined CHIP_6654 #define PLATFORM_BASE_CLK_RATE_MHZ (67) # else #error MKSTR(__FILE__) MKSTR(__LINE__) #endif /* PREDIV */ #define PLATFORM_PLL_PREDIV_val (1) /* POSTDIV */ #define PLATFORM_PLL_POSTDIV_val (2) /* Default PLL PLLM value (100 * 20/(1*2)) = 1.0GHz) */ # if defined CHIP_6657 //FIXME: set the correct values #define PLATFORM_PLL1_PLLM_val (20) /* Default PLL PLLD value for 1.0GHz) */ #define PLATFORM_PLL1_PLLD_val (1) # elif defined CHIP_6654 #define PLATFORM_PLL1_PLLM_val (25) /* Default PLL PLLD value for 850GHz) */ #define PLATFORM_PLL1_PLLD_val (1) # else #error MKSTR(__FILE__) MKSTR(__LINE__) #endif /* Default UART baudrate value */ #define PLATFORM_UART_BAUDRATE_val (19200) /* Input crystal frequency 100 MHz */ #define PLATFORM_UART_INPUT_CLOCK_RATE ((PLATFORM_BASE_CLK_RATE_MHZ * PLATFORM_PLL1_PLLM_val * 1000000)/(PLATFORM_PLL_PREDIV_val * 12 * PLATFORM_PLL1_PLLD_val)) /* SYSCLK7 = CPU_CLK/7 in Hz */ /* 1/x-rate clock for CorePac (emulation) and the ADTF module */ #define PLATFORM_PLLDIV2_val (3) /* 1/y-rate clock for system trace module only */ #define PLATFORM_PLLDIV5_val (5) /* 1/z-rate clock is used as slow_sysclck in the system */ #define PLATFORM_PLLDIV8_val (64) /* LED Definitions */ #define PLATFORM_FPGA_LED_COUNT (4) #define PLATFORM_I2C_LED_COUNT (0) #define PLATFORM_TOTAL_LED_COUNT (PLATFORM_FPGA_LED_COUNT + PLATFORM_I2C_LED_COUNT) /* Number of cores on the platform */ #define PLATFORM_CORE_COUNT 2 /* Mmeory Sections */ #define PLATFORM_L1P_BASE_ADDRESS 0x10E00000 #define PLATFORM_L1P_SIZE 0x8000 /* 32K bytes */ #define PLATFORM_L1D_BASE_ADDRESS 0x10F00000 #define PLATFORM_L1D_SIZE 0x8000 /* 32K bytes */ #define PLATFORM_DDR3_SDRAM_START 0x80000000 #define PLATFORM_DDR3_SDRAM_END 0x9FFFFFFF /* 512 MB */ /* 24AA1025 EEPROM */ #define PLATFORM_EEPROM_MANUFACTURER_ID (0x01) #define PLATFORM_EEPROM_DEVICE_ID_1 (0x50) #define PLATFORM_EEPROM_DEVICE_ID_2 (0x51) /******************************************************************************************** * General Declarations * *******************************************************************************************/ /******************************************************************************************** * Function Prototypes * *******************************************************************************************/ #if (PLATFORM_SEMLOCK_IN) #define PLIBSPILOCK() Osal_platformSpiCsEnter(); #define PLIBSPIRELEASE() Osal_platformSpiCsExit (); #else #define PLIBSPILOCK() #define PLIBSPIRELEASE() #endif /* Function prototypes that don't live anywhere else */ //extern void configSerdes(); //extern void Init_SGMII(uint32_t macport); extern void PowerUpDomains (void); extern void xmc_setup(); /******************************************************************************************** * PLL control local Declarations * *******************************************************************************************/ /** * Handle to access BOOTCFG registers. */ #define hPscCfg ((CSL_PscRegs*)CSL_PSC_REGS) #define hPllcRegs ((CSL_PllcRegs*)CSL_PLL_CONTROLLER_REGS) #define BWADJ_BIT_SHIFT 24 #define BYPASS_BIT_SHIFT 23 #define CLKF_BIT_SHIFT 6 #define ENSAT_BIT_SHIFT 6 #define RESET_BIT_SHIFT 14 /* DDR3 PLL settings for 1333 MHz */ //NOTE: //CLK = CLKIN × (PLLM+1) ÷ (OUTPUT_DIVIDE × (PLLD+1)) # if defined CHIP_6657 #define PLLM_DDR3 39 #define PLLD_DDR3 2 # elif defined CHIP_6654 #define PLLM_DDR3 59 #define PLLD_DDR3 2 # else #error MKSTR(__FILE__) MKSTR(__LINE__) # endif
Thank you in advance
George