Hi,
I have questions about 66AK2H06 DDR3 memory controller.
I'm having a problem that value of DX6LCDLR2 register are not constant.
Sometime the value will be 0x57 but sometimes it will be 0x25.
I have following queston:
Q1.
Are the value of DX6LCDLR2 register the result of READ DQS gate training?
Q2.
If anwser of Q1 is yes, I want to check the signal durning the training.
Is it available to start only READ DQS gate training by setting QSGATE bit of PHY Initialization Register?
Q3.
As I mention above, the value of DX6LCDLR2 register is fluctuating.
Is this means that the time between submitting read commands and getting the response data are fluctuating?
best regards,
g.f.