Other Parts Discussed in Thread: DM3730
Hi,
I'm trying to get startet with the Zoom Torpedo DM3730 Development from LogicPD. So far I got my toolchains in CCSv5.3 running, and I could build and successfully run basic applications. (Hello World! on ARM and DSP Side) Now I'm in great trouble getting startet with the development in the directions SYS/BIOS on ARM or DSP, communication and booting.
Final target is an application with control structure on ARM and high-speed image processing on DSP (fps > 1kHz)
Basic Questions are:
-
Is it possible to execute SYS/BIOS on the DSP? What about debugging? (We build SYS/BIOS for DSP, loaded and got no output/feedback about the status)
-
We successfully launched SYS/BIOS on the ARM, debugging inclusive. How can we boot SYS/BIOS out of the Flash/ NAND? (Which data should downloaded to which address, which configuration is needed in CCSv5?
-
How to launch applications from SYS/BIOS on ARM into the DSP?
Some information about the enviroment:
Zoom Torpedo DM3730 Development Kit Logic PD
Blackhawk USB100v2 JTAG Emulator
CCS 5.3 Win7 64bit
C6000_7.4.1 and ARM_5.0.1
It would be very helpful if anybody would have a whole ccs project demonstrating the named tasks.
best regards
Pay Gießelmann