This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Zoom Torpedo DM3730 Development Kit Getting Startet

Other Parts Discussed in Thread: DM3730

Hi,

I'm trying to get startet with the Zoom Torpedo DM3730 Development from LogicPD. So far I got my toolchains in CCSv5.3 running, and I could build and successfully run basic applications. (Hello World! on ARM and DSP Side) Now I'm in great trouble getting startet with the development in the directions SYS/BIOS on ARM or DSP, communication and booting.

Final target is an application with control structure on ARM and high-speed image processing on DSP (fps > 1kHz)

Basic Questions are:

  1. Is it possible to execute SYS/BIOS on the DSP? What about debugging? (We build SYS/BIOS for DSP, loaded and got no output/feedback about the status)

  2. We successfully launched SYS/BIOS on the ARM, debugging inclusive. How can we boot SYS/BIOS out of the Flash/ NAND? (Which data should downloaded to which address, which configuration is needed in CCSv5?

  3. How to launch applications from SYS/BIOS on ARM into the DSP?

Some information about the enviroment:

Zoom Torpedo DM3730 Development Kit Logic PD

Blackhawk USB100v2 JTAG Emulator

CCS 5.3 Win7 64bit

C6000_7.4.1 and ARM_5.0.1

It would be very helpful if anybody would have a whole ccs project demonstrating the named tasks.

best regards

Pay Gießelmann