This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 with 2GB DDR3 on board. MCFW compilation failed

3858.dvr_rdk_c6xdsp_debug_2048M_512M.xe674.txtHello TI' teams.

I have developed customer board for DM8148 and 2GB physical memory on board.
As software I use MCFW version 3.5 from ud-works.
My customer board have DM8148 (PG3.0) and 2GB of DDR3 memory.
DDR memory test by Jtag and DDR write leveling both work fine on my board.

MCFW compiled successfully when I use memory configuration file for 512MB supplied by ud-works
Bu, when I tried create new memory configuration file for 2GB and rebuild MCFW with it I have a very strange error:

After execute "make sys_all" and after u-boot, kernel and syslink successfull compilation:
===============================================================================
...
error #10281-D: Section ".bss" requires a STATIC_BASE relative relocation, but
   is located at 0xc1649000, which is probably out of range of the STATIC_BASE.
   STATIC_BASE is located at 0xc1649000. Might be required to correct
   placement of ".bss" so it lies within 0x8000 of the STATIC_BASE.
error #10281-D: Section ".neardata" requires a STATIC_BASE relative relocation,
   but is located at 0xc171e084, which is probably out of range of the
   STATIC_BASE. STATIC_BASE is located at 0xc1649000. Might be required to
   correct   placement of ".neardata" so it lies within 0x8000 of the
   STATIC_BASE.
error #10281-D: Section ".rodata" requires a STATIC_BASE relative relocation,
   but is located at 0xc171e0c0, which is probably out of range of the
   STATIC_BASE. STATIC_BASE is located at 0xc1649000. Might be required to
   correct   placement of ".rodata" so it lies within 0x8000 of the
   STATIC_BASE.
error #10010: errors encountered during linking;
   "/home/marat/workdir/SmartCore/trunk/dvr_rdk/build/dvr_rdk/bin/ti814x-scp/dv
   r_rdk_c6xdsp_debug_2048M_512M.xe674" not built
....
=================================================================================


Please help me to fix this problem.
I don't clearly understood where is STATIC_BASE defined and what I need to change on Sys/BIOS level for complete compile my code.

My memory configuration file attached. Please just rename "config_2G.txt" to "config_2G.bld"

/*
 *  ======== config.bld ========
 *  Build configuration script for HDVPSS drivers
 */

/* load the required modules for the configuration */

var M3 = xdc.useModule('ti.targets.arm.elf.M3');
var C674 = xdc.useModule('ti.targets.elf.C674');

var buildReleaseConfig = true;

/* configure  the options for the M3 targets     */

/* M3 compiler directory path                    */
M3.rootDir = java.lang.System.getenv("CGTOOLS");

/* linker options */

M3.lnkOpts.suffix += " --zero_init=off ";
M3.lnkOpts.suffix += " --dynamic --retain=_Ipc_ResetVector";

/* compiler options                                */
M3.ccOpts.suffix += "  --gcc -DTI_814X_BUILD -DPLATFORM_EVM_SI -DSYSLINK_BUILD_RTOS -DUSE_SYSLINK_NOTIFY=0 -DUTILS_ASSERT_ENABLE -DSCP_DDR_MEM_SIZE_2G";

/* set default platform and list of all interested
 * platforms for M3
 */
M3.platforms = [
                        "ti.platforms.evmTI814X:core0",
                        "ti.platforms.evmTI814X:core1",
               ];

/* Select the default platform
 *
 * Making core1 as defualt core configuration to be used
 *  Core 0 ==    Ducati.M3.VIDEO
 *  Core 1 ==    Ducati.M3.VPS
 */
M3.platform = M3.platforms[1];

/* configure  the options for the C674 targets     */

/* C674 compiler directory path                    */
C674.rootDir = java.lang.System.getenv("CGTOOLS_DSP");

/* linker options */

C674.lnkOpts.suffix += " --zero_init=off ";
C674.lnkOpts.suffix += " --dynamic --retain=_Ipc_ResetVector";

/* compiler options                                */
C674.ccOpts.suffix += " -DTI_814X_BUILD -DPLATFORM_EVM_SI -DSYSLINK_BUILD_RTOS -DUSE_SYSLINK_NOTIFY=0";

C674.platforms = ["ti.platforms.evmTI816X:plat"];
C674.platform = C674.platforms[0];

/* list interested targets in Build.targets array  */
Build.targets = [
                    M3,
                    C674,
                ];



var KB=1024;
var MB=KB*KB;
var GB=KB*KB*KB;

var DDR3_ADDR            = 0x80000000;
var DDR3_SIZE            = 2048*MB;
var DDR3_ADDR_REG0_START = 0x80000000;
var DDR3_ADDR_REG0_END   = 0xBFFFFFFF;
var DDR3_ADDR_REG1_START = 0xC0000000;
var DDR3_ADDR_REG1_END   = 0xFFFFFFFF;



var OCMC0_ADDR                 = 0x40300000;
/*OCMC1 exisits only for TI816X*/
var OCMC1_ADDR                 = 0x40400000;
var OCMC_SIZE                  = 128*KB;

var OCMC0_VIDEO_M3_SIZE        = 16*KB;
var OCMC0_VPSS_M3_SIZE         = OCMC_SIZE - OCMC0_VIDEO_M3_SIZE;

var OCMC0_VIDEO_M3_ADDR        = OCMC0_ADDR;
var OCMC0_VPSS_M3_ADDR          = OCMC0_VIDEO_M3_ADDR + OCMC0_VIDEO_M3_SIZE;



var OCMC0_RUN_ADDR             = 0x00300000;
var OCMC0_VIDEO_M3_RUN         = OCMC0_RUN_ADDR;
var OCMC0_VPSS_M3_RUN          = OCMC0_VIDEO_M3_RUN + OCMC0_VIDEO_M3_SIZE;

var M3_L2_RAM              = 0x55024000;
var M3_L2_RAM_SIZE         = 48*KB;

var M3_L2_RAM_MAPPED          = 0x20004000;

var TOTAL_MEM_SIZE             = 2048*MB;

/* =================================== */
/* FIRST 512MB */
var SR1_SIZE                   = 384*MB;
var VIDEO_M3_CODE_SIZE         = 8*MB 
var VIDEO_M3_DATA_SIZE         = 24*MB;
var VIDEO_M3_BSS_SIZE          = 32*MB;
var DSS_M3_CODE_SIZE           = 8*MB;
var DSS_M3_DATA_SIZE           = 24*MB;
var DSS_M3_BSS_SIZE            = 32*MB
/* =================================== */

/* =================================== */
/* SECOND 512MB */
var TILER_SIZE                 = 256*MB; /* MUST be aligned on 128MB boundary */
var SR2_FRAME_BUFFER_SIZE      = 256*MB;  
/* =================================== */

/* =================================== */
/* THIRD 512MB */
var DSP_CODE_SIZE              = 16*MB;
var DSP_DATA_SIZE              = 476*MB;
var SR0_SIZE                   = 12*MB;
var VIDEO_M3_EXCEPTION_CTX_SIZE = 512*KB;
var VPSS_M3_EXCEPTION_CTX_SIZE = 512*KB;
var HDVPSS_DESC_SIZE           = 2*MB;
var HDVPSS_SHARED_SIZE         = 2*MB;
var NOTIFY_SHARED_SIZE         = 2*MB;
var REMOTE_DEBUG_SIZE          = 1*MB;
/* =================================== */

/* =================================== */
/* LAST 512 MB */
var LINUX_SIZE                 = 512*MB;
/* =================================== */


print ("                                                         "); 
print ("SmartCore Memory Map - 2GB DDR [4 x 512MB regions], 512MB for Linux:");
print ("                                                         "); 
print ("  0x80000000 ----+-------------------+");
print ("         ^       |  " + (SR1_SIZE / MB) + "MB            | (SR1) Bitstream buffer");
print ("         |       |                   | Cached on A8. Cached on M3, although access by DMAs");
print ("         |       +-------------------+ ");
print ("         |       |   " + (VIDEO_M3_CODE_SIZE / MB) + " MB            | Video M3 Code");
print ("       512MB     +-------------------+");
print ("         |       |   " + (VIDEO_M3_DATA_SIZE / MB) + " MB           | Video  M3 Data");
print ("         |       +-------------------+");
print ("         |       |   " + (DSS_M3_CODE_SIZE/ MB) + " MB            | VPSS  M3 Code");
print ("         |       +-------------------+");
print ("         v       |   " + (DSS_M3_DATA_SIZE/ MB) + " MB           | VPSS  M3 Data");
print ("  0xA0000000 ----+-------------------+");
print ("         ^       |                   |");
print ("         |       |   " + (TILER_SIZE / MB) + " MB          | Tiled 8-bit + 16-bit region");
print ("       512MB     |                   |");
print ("         |       +-------------------+");
print ("         v       |  "  + (SR2_FRAME_BUFFER_SIZE / MB) + " MB           | (SR2) Frame Buffer Region - <VPSS - Video M3 Frame Buf>");
print ("  0xC0000000 ----+-------------------+  ");
print ("         ^       |   " + ( DSP_CODE_SIZE / KB) + " KB         | DSP Code");
print ("         |       +-------------------+");
print ("         |       |   " + (DSP_DATA_SIZE / MB) + " MB          | DSP Data");
print ("         |       +-------------------+");
print ("         |       |                   |");
print ("       512MB     |  " + (SR0_SIZE / MB) + " MB            | (SR0) Syslink MsgQ/IPC List MP - <Non-cached on M3>");
print ("         |       +-------------------+");
print ("         |       |  " + (VIDEO_M3_EXCEPTION_CTX_SIZE / KB) + " KB           | Video M3 exception context");
print ("         |       +-------------------+  ");
print ("         |       |  " + (VPSS_M3_EXCEPTION_CTX_SIZE / KB) + "KB            | Vpss M3 exception context");
print ("         |       +-------------------+  ");
print ("         |       |  " + (HDVPSS_DESC_SIZE / MB) + " MB             | VPSS M3 - VPDMA Descriptor");
print ("         |       +-------------------+");
print ("         |       |  " + (HDVPSS_SHARED_SIZE / MB) + " MB             | VPSS M3 - FBDev Shared Memory");
print ("         |       +-------------------+");
print ("         |       |  " + (NOTIFY_SHARED_SIZE / MB) + " MB             | Host - VPSS M3 Notify(For FBDev)");
print ("         |       +-------------------+");
print ("         v       |  " + (REMOTE_DEBUG_SIZE / MB) + " MB             | Remote Debug Print");
print ("  0xE0000000 ----+-------------------+");
print ("         ^       |                   |");
print ("         |       |  " + (LINUX_SIZE / MB) + " MB           | Linux");
print ("       512MB     |                   |");
print ("         |       |                   |"); 
print ("         v       |                   |");
print ("  0xFFFFFFFF ----+-------------------+");  
print ("                                                         "); 

var SR1_ADDR                   = DDR3_ADDR_REG0_START;
var VIDEO_M3_CODE_ADDR         = SR1_ADDR                   + SR1_SIZE;
var VIDEO_M3_DATA_ADDR         = VIDEO_M3_CODE_ADDR         + VIDEO_M3_CODE_SIZE;
var VIDEO_M3_BSS_ADDR          = VIDEO_M3_DATA_ADDR         + VIDEO_M3_DATA_SIZE;

/*
    VIDEO_M3_BSS_ADDR_RUN is the translated address for VIDEO_M3_BSS_ADDR in the 
    0x20000000 region. Its assumed VIDEO_M3_BSS_ADDR lies in 0x80000000 region
*/
var VIDEO_M3_BSS_ADDR_RUN      = VIDEO_M3_BSS_ADDR - DDR3_ADDR + 0x20000000;
 
var DSS_M3_CODE_ADDR          = VIDEO_M3_BSS_ADDR         + VIDEO_M3_BSS_SIZE;
var DSS_M3_DATA_ADDR          = DSS_M3_CODE_ADDR           + DSS_M3_CODE_SIZE;
var DSS_M3_BSS_ADDR           = DSS_M3_DATA_ADDR           + DSS_M3_DATA_SIZE;
var DSS_M3_BSS_RUN            = DSS_M3_BSS_ADDR - DDR3_ADDR + 0x20000000;

var TILER_ADDR                  = DSS_M3_BSS_ADDR + DSS_M3_BSS_SIZE;
var SR2_FRAME_BUFFER_ADDR       = TILER_ADDR                    + TILER_SIZE;

var DSP_CODE_ADDR             = DDR3_ADDR_REG1_START;
var DSP_DATA_ADDR             = DSP_CODE_ADDR              + DSP_CODE_SIZE;
if ((DSP_DATA_ADDR + DSP_DATA_SIZE) > DDR3_ADDR_REG1_END)
{
  throw xdc.$$XDCException("MEMORY_MAP OVERFLOW ERROR ",
                           "\nRegion End: " + "0x" + java.lang.Long.toHexString(DDR3_ADDR_REG1_END) + 
                           "\nActual End: " + "0x" + java.lang.Long.toHexString(DSP_DATA_ADDR + DSP_DATA_SIZE));
}

var SR0_ADDR                    = DSP_DATA_ADDR               + DSP_DATA_SIZE;
var VIDEO_M3_EXCEPTION_CTX_ADDR = SR0_ADDR                    + SR0_SIZE;
var VPSS_M3_EXCEPTION_CTX_ADDR  = VIDEO_M3_EXCEPTION_CTX_ADDR + VIDEO_M3_EXCEPTION_CTX_SIZE;
var HDVPSS_DESC_ADDR            = VPSS_M3_EXCEPTION_CTX_ADDR  + VPSS_M3_EXCEPTION_CTX_SIZE;
var HDVPSS_SHARED_ADDR          = HDVPSS_DESC_ADDR            + HDVPSS_DESC_SIZE;
var NOTIFY_SHARED_ADDR          = HDVPSS_SHARED_ADDR          + HDVPSS_SHARED_SIZE;
var REMOTE_DEBUG_ADDR           = NOTIFY_SHARED_ADDR          + NOTIFY_SHARED_SIZE;

if ((VPSS_M3_EXCEPTION_CTX_ADDR + VPSS_M3_EXCEPTION_CTX_SIZE) > HDVPSS_SHARED_ADDR)
{
  print(" ### DSP_CODE_ADDR                    = " + java.lang.Long.toHexString(DSP_CODE_ADDR));
  print(" ### DSP_DATA_ADDR                    = " + java.lang.Long.toHexString(DSP_DATA_ADDR));
  print(" ### SR0_ADDR                         = " + java.lang.Long.toHexString(SR0_ADDR));
  print(" ### VIDEO_M3_EXCEPTION_CTX_ADDR      = " + java.lang.Long.toHexString(VIDEO_M3_EXCEPTION_CTX_ADDR));
  print(" ### VPSS_M3_EXCEPTION_CTX_ADDR       = " + java.lang.Long.toHexString(VP0SS_M3_EXCEPTION_CTX_ADDR));
  print(" ### HDVPSS_DESC_ADDR                 = " + java.lang.Long.toHexString(HDVPSS_DESC_ADDR));
  print(" ### HDVPSS_SHARED_ADDR               = " + java.lang.Long.toHexString(HDVPSS_SHARED_ADDR));
   
  throw xdc.$$XDCException("MEMORY_MAP OVERFLOW ERROR ",
                           "\nRegion End: " + "0x" + java.lang.Long.toHexString(SR0_ADDR + SR0_SIZE) + 
                           "\nActual End: " + "0x" + java.lang.Long.toHexString(HDVPSS_DESC_ADDR ));
}

var LINUX_ADDR                 = REMOTE_DEBUG_ADDR + REMOTE_DEBUG_SIZE;


/*
if ((REMOTE_DEBUG_ADDR + REMOTE_DEBUG_SIZE) > (DDR3_ADDR_REG1_END - LINUX_SIZE + 1))
{
  throw xdc.$$XDCException("MEMORY_MAP OVERFLOW ERROR ",
                           "\nRegion End: " + "0x" + java.lang.Long.toHexString(DDR3_ADDR_REG1_END) + 
                           "\nActual End: " + "0x" + java.lang.Long.toHexString(REMOTE_DEBUG_ADDR + REMOTE_DEBUG_SIZE ));
}
*/

var TOTAL_DDR_USED_SIZE_IN_MB  = ((((REMOTE_DEBUG_ADDR + REMOTE_DEBUG_SIZE) - DDR3_ADDR_REG1_START)) + ((DSP_DATA_ADDR + DSP_DATA_SIZE) - DDR3_ADDR_REG1_START))/MB;

print(" ### ");
print(" ### REGIONS MAP: ###");
print(" ======== First 512 MB: ================================= ");
print(" ### SR1:                         0x" + java.lang.Long.toHexString(SR1_ADDR) + " - 0x" + java.lang.Long.toHexString(SR1_ADDR+SR1_SIZE));
print(" ### VIDEO_M3_CODE_ADDR:          0x" + java.lang.Long.toHexString(VIDEO_M3_CODE_ADDR) + " - 0x" + java.lang.Long.toHexString(VIDEO_M3_CODE_ADDR+VIDEO_M3_CODE_SIZE));
print(" ### VIDEO_M3_DATA_ADDR:          0x" + java.lang.Long.toHexString(VIDEO_M3_DATA_ADDR) + " - 0x" + java.lang.Long.toHexString(VIDEO_M3_DATA_ADDR+VIDEO_M3_DATA_SIZE));
print(" ### DSS_M3_CODE_ADDR:            0x" + java.lang.Long.toHexString(DSS_M3_CODE_ADDR) + " - 0x" + java.lang.Long.toHexString(DSS_M3_CODE_ADDR+DSS_M3_CODE_SIZE));
print(" ### DSS_M3_DATA_ADDR:            0x" + java.lang.Long.toHexString(DSS_M3_DATA_ADDR) + " - 0x" + java.lang.Long.toHexString(DSS_M3_DATA_ADDR+DSS_M3_DATA_SIZE));
print(" ======== Second 512 MB: ================================= ");
print(" ### TILER_ADDR:                  0x" + java.lang.Long.toHexString(TILER_ADDR) + " - 0x" + java.lang.Long.toHexString(TILER_ADDR+TILER_SIZE));
print(" ### SR2_FRAME_BUFFER_ADDR:       0x" + java.lang.Long.toHexString(SR2_FRAME_BUFFER_ADDR) + " - 0x" + java.lang.Long.toHexString(SR2_FRAME_BUFFER_ADDR+SR2_FRAME_BUFFER_SIZE));
print(" ========= Third 512 MB: ================================== ");
print(" ### DSP_CODE_ADDR:               0x" + java.lang.Long.toHexString(DSP_CODE_ADDR) + " - 0x" + java.lang.Long.toHexString(DSP_CODE_ADDR+DSP_CODE_SIZE));
print(" ### DSP_DATA_ADDR:               0x" + java.lang.Long.toHexString(DSP_DATA_ADDR) + " - 0x" + java.lang.Long.toHexString(DSP_DATA_ADDR+DSP_DATA_SIZE));
print(" ### SR0_ADDR:                    0x" + java.lang.Long.toHexString(SR0_ADDR) + " - 0x" + java.lang.Long.toHexString(SR0_ADDR+SR0_SIZE));
print(" ### VIDEO_M3_EXCEPTION_CTX_ADDR: 0x" + java.lang.Long.toHexString(VIDEO_M3_EXCEPTION_CTX_ADDR) + " - 0x" + java.lang.Long.toHexString(VIDEO_M3_EXCEPTION_CTX_ADDR+VIDEO_M3_EXCEPTION_CTX_SIZE));
print(" ### VPSS_M3_EXCEPTION_CTX_ADDR:  0x" + java.lang.Long.toHexString(VPSS_M3_EXCEPTION_CTX_ADDR) + " - 0x" + java.lang.Long.toHexString(VPSS_M3_EXCEPTION_CTX_ADDR+VPSS_M3_EXCEPTION_CTX_SIZE));
print(" ### HDVPSS_DESC_ADDR:            0x" + java.lang.Long.toHexString(HDVPSS_DESC_ADDR) + " - 0x" + java.lang.Long.toHexString(HDVPSS_DESC_ADDR+HDVPSS_DESC_SIZE));
print(" ### HDVPSS_SHARED_ADDR:          0x" + java.lang.Long.toHexString(HDVPSS_SHARED_ADDR) + " - 0x" + java.lang.Long.toHexString(HDVPSS_SHARED_ADDR+HDVPSS_SHARED_SIZE));
print(" ### NOTIFY_SHARED_ADDR:          0x" + java.lang.Long.toHexString(NOTIFY_SHARED_ADDR) + " - 0x" + java.lang.Long.toHexString(NOTIFY_SHARED_ADDR+NOTIFY_SHARED_SIZE));
print(" ### REMOTE_DEBUG_ADDR:           0x" + java.lang.Long.toHexString(REMOTE_DEBUG_ADDR) + " - 0x" + java.lang.Long.toHexString(REMOTE_DEBUG_ADDR+REMOTE_DEBUG_SIZE));
print(" ======== Last 512 MB: ================================== ");
print(" ### LINUX:                       0x" + java.lang.Long.toHexString(LINUX_ADDR) + " - 0x" + java.lang.Long.toHexString(LINUX_ADDR+LINUX_SIZE-1));
print(" ========================================================= ");
print(" ### ");
print(" ========================================================= ");
print(" ### Total DDR usage in MB = " + TOTAL_DDR_USED_SIZE_IN_MB + " MB ###");
print(" ========================================================= ");
print(" ### ");

Build.platformTable["ti.platforms.evmTI814X:core1"] =
{
    externalMemoryMap:
    [
        ["DDR3_RAM", {
            comment: "DDR3_RAM",
            name: "DDR3_RAM",
            base: DDR3_ADDR,
            len:  DDR3_SIZE
        }],
        ["OCMC0_RAM", {
            comment: "OCMC0_RAM",
            name: "OCMC0_RAM",
            base: OCMC0_ADDR,
            len:  OCMC_SIZE
        }],
        ["OCMC1_RAM", {
            comment: "OCMC1_RAM",
            name: "OCMC1_RAM",
            base: OCMC1_ADDR,
            len:  OCMC_SIZE
        }],
        ["M3_L2_RAM", {
            comment: "M3_L2_RAM",
            name: "M3_L2_RAM",
            base: M3_L2_RAM,
            len:  M3_L2_RAM_SIZE
        }],
        ["OCMC0_RAM_MAPPED", {
            comment: "OCMC0_RAM",
            name: "OCMC0_RAM_MAPPED",
            base: OCMC0_RUN_ADDR,
            len:  OCMC_SIZE
        }],         
        ["CACHE_WB_DDR_LOGICAL_ADDRESS", {
            comment: "CACHE_WB_DDR_LOGICAL_ADDRESS",
            name: "CACHE_WB_DDR_LOGICAL_ADDRESS",
            base: 0x20000000,
            len:  0x20000000,
        }],       
    ],
    customMemoryMap:
    [
        ["LINUX_MEM", {
            comment : "LINUX_MEM",
            name    : "LINUX_MEM",
            base    : LINUX_ADDR,
            len     : LINUX_SIZE
        }],
        ["SR1", {
            comment : "SR1",
            name    : "SR1",
            base    : SR1_ADDR,
            len     : SR1_SIZE
        }],
        ["VIDEO_M3_CODE_MEM", {
            comment : "VIDEO_M3_CODE_MEM",
            name    : "VIDEO_M3_CODE_MEM",
            base    : VIDEO_M3_CODE_ADDR,
            len     : VIDEO_M3_CODE_SIZE
        }],
        ["VIDEO_M3_DATA_MEM", {
            comment : "VIDEO_M3_DATA_MEM",
            name    : "VIDEO_M3_DATA_MEM",
            base    : VIDEO_M3_DATA_ADDR,
            len     : VIDEO_M3_DATA_SIZE
        }],
        ["VIDEO_M3_BSS_ADDR", {
            comment : "VIDEO_M3_BSS_ADDR",
            name    : "VIDEO_M3_BSS_ADDR",
            base    : VIDEO_M3_BSS_ADDR,
            len     : VIDEO_M3_BSS_SIZE
        }],
        ["VIDEO_M3_BSS_ADDR_RUN", {
            comment : "VIDEO_M3_BSS_ADDR_RUN",
            name    : "VIDEO_M3_BSS_ADDR_RUN",
            base    : VIDEO_M3_BSS_ADDR_RUN,
            len     : VIDEO_M3_BSS_SIZE
        }],
        ["DSS_M3_CODE_MEM", {
            comment : "DSS_M3_CODE_MEM",
            name    : "DSS_M3_CODE_MEM",
            base    : DSS_M3_CODE_ADDR,
            len     : DSS_M3_CODE_SIZE
        }],
        ["DDR3_M3", {
            comment : "DDR3_M3",
            name    : "DDR3_M3",
            base    : DSS_M3_DATA_ADDR,
            len     : DSS_M3_DATA_SIZE
        }],
        ["DSS_M3_BSS_ADDR", {
            comment : "DSS_M3_BSS_ADDR",
            name    : "DSS_M3_BSS_ADDR",
            base    : DSS_M3_BSS_ADDR,
            len     : DSS_M3_BSS_SIZE
        }],        
        ["DSS_M3_BSS_ADDR_RUN", {
            comment : "DSS_M3_BSS_ADDR_RUN",
            name    : "DSS_M3_BSS_ADDR_RUN",
            base    : DSS_M3_BSS_RUN,
            len     : DSS_M3_BSS_SIZE
        }],        
         ["TILER_MEM", {
            comment : "TILER_MEM",
            name    : "TILER_MEM",
            base    : TILER_ADDR,
            len     : TILER_SIZE
        }],
        ["SR2_FRAME_BUFFER_MEM", {
            comment : "SR2_FRAME_BUFFER_MEM",
            name    : "SR2_FRAME_BUFFER_MEM",
            base    : SR2_FRAME_BUFFER_ADDR,
            len     : SR2_FRAME_BUFFER_SIZE
        }],
        ["SR0", {
            comment : "SR0",
            name    : "SR0",
            base    : SR0_ADDR,
            len     : SR0_SIZE
        }],
        ["VIDEO_M3_EXCEPTION_CTX", {
            comment : "VIDEO_M3_EXCEPTION_CTX",
            name    : "VIDEO_M3_EXCEPTION_CTX",
            base    : VIDEO_M3_EXCEPTION_CTX_ADDR,
            len     : VIDEO_M3_EXCEPTION_CTX_SIZE
        }],
        ["VPSS_M3_EXCEPTION_CTX", {
            comment : "VPSS_M3_EXCEPTION_CTX",
            name    : "VPSS_M3_EXCEPTION_CTX",
            base    : VPSS_M3_EXCEPTION_CTX_ADDR,
            len     : VPSS_M3_EXCEPTION_CTX_SIZE
        }],
        ["HDVPSS_DESC_MEM", {
            comment : "HDVPSS_DESC_MEM",
            name    : "HDVPSS_DESC_MEM",
            base    : HDVPSS_DESC_ADDR,
            len     : HDVPSS_DESC_SIZE
        }],
        ["HDVPSS_SHARED_MEM", {
            comment : "HDVPSS_SHARED_MEM",
            name    : "HDVPSS_SHARED_MEM",
            base    : HDVPSS_SHARED_ADDR,
            len     : HDVPSS_SHARED_SIZE
        }],
        ["HOST_VPSS_NOTIFYMEM", {
            comment : "HOST_VPSS_NOTIFYMEM",
            name    : "HOST_VPSS_NOTIFYMEM",
            base    : NOTIFY_SHARED_ADDR,
            len     : NOTIFY_SHARED_SIZE
        }],
        ["REMOTE_DEBUG_MEM", {
            comment : "REMOTE_DEBUG_MEM",
            name    : "REMOTE_DEBUG_MEM",
            base    : REMOTE_DEBUG_ADDR,
            len     : REMOTE_DEBUG_SIZE
        }],
        ["L2_ROM", {
            comment: "L2_ROM",
            name: "L2_ROM",
            base: 0x00000000,
            len:  0x00004000
        }],
        ["OCMC0_VIDEO_M3_RAM", {
            comment: "OCMC0_VIDEO_M3_RAM",
            name: "OCMC0_VIDEO_M3_RAM",
            base: OCMC0_VIDEO_M3_ADDR,
            len:  OCMC0_VIDEO_M3_SIZE
        }],
        ["OCMC0_VPSS_M3_RAM", {
            comment: "OCMC0_VPSS_M3_RAM",
            name: "OCMC0_VPSS_M3_RAM",
            base: OCMC0_VPSS_M3_ADDR,
            len:  OCMC0_VPSS_M3_SIZE
        }],        
        ["OCMC1_RAM", {
            comment: "OCMC1_RAM",
            name: "OCMC1_RAM",
            base: OCMC1_ADDR,
            len:  OCMC_SIZE
        }],
        ["M3_L2_RAM", {
            comment: "M3_L2_RAM",
            name: "M3_L2_RAM",
            base: M3_L2_RAM,
            len:  M3_L2_RAM_SIZE
        }],
        ["M3_L2_RAM_MAPPED", {
            comment: "M3_L2_RAM",
            name: "M3_L2_RAM_MAPPED",
            base: M3_L2_RAM_MAPPED,
            len:  M3_L2_RAM_SIZE
        }],
        ["OCMC0_VIDEO_M3_RAM_MAPPED", {
            comment: "OCMC0_VIDEO_M3_RAM_MAPPED",
            name: "OCMC0_VIDEO_M3_RAM_MAPPED",
            base: OCMC0_VIDEO_M3_RUN,
            len:  OCMC0_VIDEO_M3_SIZE
        }],
        ["OCMC0_VPSS_M3_RAM_MAPPED", {
            comment: "OCMC0_VPSS_M3_RAM_MAPPED",
            name: "OCMC0_VPSS_M3_RAM_MAPPED",
            base: OCMC0_VPSS_M3_RUN,
            len:  OCMC0_VPSS_M3_SIZE
        }], 
    ]
};

Build.platformTable["ti.platforms.evmTI814X:core0"] =
{
    externalMemoryMap:
    [
        ["DDR3_RAM", {
            comment: "DDR3_RAM",
            name: "DDR3_RAM",
            base: DDR3_ADDR,
            len:  DDR3_SIZE
        }],
        ["OCMC0_RAM", {
            comment: "OCMC0_RAM",
            name: "OCMC0_RAM",
            base: OCMC0_ADDR,
            len:  OCMC_SIZE
        }],
        ["OCMC1_RAM", {
            comment: "OCMC1_RAM",
            name: "OCMC1_RAM",
            base: OCMC1_ADDR,
            len:  OCMC_SIZE
        }],
        ["M3_L2_RAM", {
            comment: "M3_L2_RAM",
            name: "M3_L2_RAM",
            base: M3_L2_RAM,
            len:  M3_L2_RAM_SIZE
        }],   
       ["OCMC0_RAM_MAPPED", {
            comment: "OCMC0_RAM",
            name: "OCMC0_RAM_MAPPED",
            base: OCMC0_RUN_ADDR,
            len:  OCMC_SIZE
        }],
        ["CACHE_WB_DDR_LOGICAL_ADDRESS", {
            comment: "CACHE_WB_DDR_LOGICAL_ADDRESS",
            name: "CACHE_WB_DDR_LOGICAL_ADDRESS",
            base: 0x20000000,
            len:  0x20000000,
        }],          
        
    ],
    customMemoryMap:
    [
        ["LINUX_MEM", {
            comment : "LINUX_MEM",
            name    : "LINUX_MEM",
            base    : LINUX_ADDR,
            len     : LINUX_SIZE
        }],
        ["SR1", {
            comment : "SR1",
            name    : "SR1",
            base    : SR1_ADDR,
            len     : SR1_SIZE
        }],
        ["VIDEO_M3_CODE_MEM", {
            comment : "VIDEO_M3_CODE_MEM",
            name    : "VIDEO_M3_CODE_MEM",
            base    : VIDEO_M3_CODE_ADDR,
            len     : VIDEO_M3_CODE_SIZE
        }],
        ["DDR3_M3", {
            comment : "DDR3_M3",
            name    : "DDR3_M3",
            base    : VIDEO_M3_DATA_ADDR,
            len     : VIDEO_M3_DATA_SIZE
        }],
        ["VIDEO_M3_BSS_ADDR", {
            comment : "VIDEO_M3_BSS_ADDR",
            name    : "VIDEO_M3_BSS_ADDR",
            base    : VIDEO_M3_BSS_ADDR,
            len     : VIDEO_M3_BSS_SIZE
        }],          
        ["VIDEO_M3_BSS_ADDR_RUN", {
            comment : "VIDEO_M3_BSS_ADDR_RUN",
            name    : "VIDEO_M3_BSS_ADDR_RUN",
            base    : VIDEO_M3_BSS_ADDR_RUN,
            len     : VIDEO_M3_BSS_SIZE
        }],          
        ["DSS_M3_CODE_MEM", {
            comment : "DSS_M3_CODE_MEM",
            name    : "DSS_M3_CODE_MEM",
            base    : DSS_M3_CODE_ADDR,
            len     : DSS_M3_CODE_SIZE
        }],
        ["DSS_M3_DATA_MEM", {
            comment : "DSS_M3_DATA_MEM",
            name    : "DSS_M3_DATA_MEM",
            base    : DSS_M3_DATA_ADDR,
            len     : DSS_M3_DATA_SIZE
        }],
        ["DSS_M3_BSS_ADDR", {
            comment : "DSS_M3_BSS_ADDR",
            name    : "DSS_M3_BSS_ADDR",
            base    : DSS_M3_BSS_ADDR,
            len     : DSS_M3_BSS_SIZE
        }],        
        ["DSS_M3_BSS_ADDR_RUN", {
            comment : "DSS_M3_BSS_ADDR_RUN",
            name    : "DSS_M3_BSS_ADDR_RUN",
            base    : DSS_M3_BSS_RUN,
            len     : DSS_M3_BSS_SIZE
        }],        

        ["TILER_MEM", {
            comment : "TILER_MEM",
            name    : "TILER_MEM",
            base    : TILER_ADDR,
            len     : TILER_SIZE
        }],
        ["SR2_FRAME_BUFFER_MEM", {
            comment : "SR2_FRAME_BUFFER_MEM",
            name    : "SR2_FRAME_BUFFER_MEM",
            base    : SR2_FRAME_BUFFER_ADDR,
            len     : SR2_FRAME_BUFFER_SIZE
        }],
        ["SR0", {
            comment : "SR0",
            name    : "SR0",
            base    : SR0_ADDR,
            len     : SR0_SIZE
        }],
        ["VIDEO_M3_EXCEPTION_CTX", {
            comment : "VIDEO_M3_EXCEPTION_CTX",
            name    : "VIDEO_M3_EXCEPTION_CTX",
            base    : VIDEO_M3_EXCEPTION_CTX_ADDR,
            len     : VIDEO_M3_EXCEPTION_CTX_SIZE
        }],
        ["VPSS_M3_EXCEPTION_CTX", {
            comment : "VPSS_M3_EXCEPTION_CTX",
            name    : "VPSS_M3_EXCEPTION_CTX",
            base    : VPSS_M3_EXCEPTION_CTX_ADDR,
            len     : VPSS_M3_EXCEPTION_CTX_SIZE
        }],
        ["HDVPSS_DESC_MEM", {
            comment : "HDVPSS_DESC_MEM",
            name    : "HDVPSS_DESC_MEM",
            base    : HDVPSS_DESC_ADDR,
            len     : HDVPSS_DESC_SIZE
        }],
        ["HDVPSS_SHARED_MEM", {
            comment : "HDVPSS_SHARED_MEM",
            name    : "HDVPSS_SHARED_MEM",
            base    : HDVPSS_SHARED_ADDR,
            len     : HDVPSS_SHARED_SIZE
        }],
        ["HOST_VPSS_NOTIFYMEM", {
            comment : "HOST_VPSS_NOTIFYMEM",
            name    : "HOST_VPSS_NOTIFYMEM",
            base    : NOTIFY_SHARED_ADDR,
            len     : NOTIFY_SHARED_SIZE
        }],
        ["REMOTE_DEBUG_MEM", {
            comment : "REMOTE_DEBUG_MEM",
            name    : "REMOTE_DEBUG_MEM",
            base    : REMOTE_DEBUG_ADDR,
            len     : REMOTE_DEBUG_SIZE
        }],
        ["L2_ROM", {
            comment: "L2_ROM",
            name: "L2_ROM",
            base: 0x00000000,
            len:  0x00004000
        }],
        ["OCMC0_VIDEO_M3_RAM", {
            comment: "OCMC0_VIDEO_M3_RAM",
            name: "OCMC0_VIDEO_M3_RAM",
            base: OCMC0_VIDEO_M3_ADDR,
            len:  OCMC0_VIDEO_M3_SIZE
        }],
        ["OCMC0_VPSS_M3_RAM", {
            comment: "OCMC0_VPSS_M3_RAM",
            name: "OCMC0_VPSS_M3_RAM",
            base: OCMC0_VPSS_M3_ADDR,
            len:  OCMC0_VPSS_M3_SIZE
        }], 
        ["OCMC1_RAM", {
            comment: "OCMC1_RAM",
            name: "OCMC1_RAM",
            base: OCMC1_ADDR,
            len:  OCMC_SIZE
        }],
        ["M3_L2_RAM", {
            comment: "M3_L2_RAM",
            name: "M3_L2_RAM",
            base: M3_L2_RAM,
            len:  M3_L2_RAM_SIZE
        }],
        ["M3_L2_RAM_MAPPED", {
            comment: "M3_L2_RAM",
            name: "M3_L2_RAM_MAPPED",
            base: M3_L2_RAM_MAPPED,
            len:  M3_L2_RAM_SIZE
        }], 
        ["OCMC0_VIDEO_M3_RAM_MAPPED", {
            comment: "OCMC0_VIDEO_M3_RAM_MAPPED",
            name: "OCMC0_VIDEO_M3_RAM_MAPPED",
            base: OCMC0_VIDEO_M3_RUN,
            len:  OCMC0_VIDEO_M3_SIZE
        }],
        ["OCMC0_VPSS_M3_RAM_MAPPED", {
            comment: "OCMC0_VPSS_M3_RAM_MAPPED",
            name: "OCMC0_VPSS_M3_RAM_MAPPED",
            base: OCMC0_VPSS_M3_RUN,
            len:  OCMC0_VPSS_M3_SIZE
        }],       
    ]
};

Build.platformTable["ti.platforms.evmTI814X:plat"] =
{
    externalMemoryMap:
    [
        ["DDR3_RAM", {
            comment: "DDR3_RAM",
            name: "DDR3_RAM",
            base: DDR3_ADDR,
            len:  DDR3_SIZE
        }],
        ["OCMC0_RAM", {
            comment: "OCMC0_RAM",
            name: "OCMC0_RAM",
            base: OCMC0_ADDR,
            len:  OCMC_SIZE
        }],
        ["OCMC1_RAM", {
            comment: "OCMC1_RAM",
            name: "OCMC1_RAM",
            base: OCMC1_ADDR,
            len:  OCMC_SIZE
        }],
    ],
    customMemoryMap:
    [
        ["LINUX_MEM", {
            comment : "LINUX_MEM",
            name    : "LINUX_MEM",
            base    : LINUX_ADDR,
            len     : LINUX_SIZE
        }],
        ["SR1", {
            comment : "SR1",
            name    : "SR1",
            base    : SR1_ADDR,
            len     : SR1_SIZE
        }],
        ["VIDEO_M3_CODE_MEM", {
            comment : "VIDEO_M3_CODE_MEM",
            name    : "VIDEO_M3_CODE_MEM",
            base    : VIDEO_M3_CODE_ADDR,
            len     : VIDEO_M3_CODE_SIZE
        }],
        ["VIDEO_M3_DATA_MEM", {
            comment : "VIDEO_M3_DATA_MEM",
            name    : "VIDEO_M3_DATA_MEM",
            base    : VIDEO_M3_DATA_ADDR,
            len     : VIDEO_M3_DATA_SIZE
        }],
        ["DSS_M3_CODE_MEM", {
            comment : "DSS_M3_CODE_MEM",
            name    : "DSS_M3_CODE_MEM",
            base    : DSS_M3_CODE_ADDR,
            len     : DSS_M3_CODE_SIZE
        }],
        ["DSS_M3_DATA_MEM", {
            comment : "DSS_M3_DATA_MEM",
            name    : "DSS_M3_DATA_MEM",
            base    : DSS_M3_DATA_ADDR,
            len     : DSS_M3_DATA_SIZE
        }],
        ["TILER_MEM", {
            comment : "TILER_MEM",
            name    : "TILER_MEM",
            base    : TILER_ADDR,
            len     : TILER_SIZE
        }],
        ["SR2_FRAME_BUFFER_MEM", {
            comment : "SR2_FRAME_BUFFER_MEM",
            name    : "SR2_FRAME_BUFFER_MEM",
            base    : SR2_FRAME_BUFFER_ADDR,
            len     : SR2_FRAME_BUFFER_SIZE
        }],
        ["DSP_CODE_MEM", {
            comment : "DSP_CODE_MEM",
            name    : "DSP_CODE_MEM",
            base    : DSP_CODE_ADDR,
            len     : DSP_CODE_SIZE
        }],
        ["DSP_DATA_MEM", {
            comment : "DDR3_DSP",
            name    : "DDR3_DSP",
            base    : DSP_DATA_ADDR,
            len     : DSP_DATA_SIZE
        }],
        ["SR0", {
            comment : "SR0",
            name    : "SR0",
            base    : SR0_ADDR,
            len     : SR0_SIZE
        }],
        ["VIDEO_M3_EXCEPTION_CTX", {
            comment : "VIDEO_M3_EXCEPTION_CTX",
            name    : "VIDEO_M3_EXCEPTION_CTX",
            base    : VIDEO_M3_EXCEPTION_CTX_ADDR,
            len     : VIDEO_M3_EXCEPTION_CTX_SIZE
        }],
        ["VPSS_M3_EXCEPTION_CTX", {
            comment : "VPSS_M3_EXCEPTION_CTX",
            name    : "VPSS_M3_EXCEPTION_CTX",
            base    : VPSS_M3_EXCEPTION_CTX_ADDR,
            len     : VPSS_M3_EXCEPTION_CTX_SIZE
        }],
        ["HDVPSS_DESC_MEM", {
            comment : "HDVPSS_DESC_MEM",
            name    : "HDVPSS_DESC_MEM",
            base    : HDVPSS_DESC_ADDR,
            len     : HDVPSS_DESC_SIZE
        }],
        ["HDVPSS_SHARED_MEM", {
            comment : "HDVPSS_SHARED_MEM",
            name    : "HDVPSS_SHARED_MEM",
            base    : HDVPSS_SHARED_ADDR,
            len     : HDVPSS_SHARED_SIZE
        }],
        ["HOST_VPSS_NOTIFYMEM", {
            comment : "HOST_VPSS_NOTIFYMEM",
            name    : "HOST_VPSS_NOTIFYMEM",
            base    : NOTIFY_SHARED_ADDR,
            len     : NOTIFY_SHARED_SIZE
        }],
        ["REMOTE_DEBUG_MEM", {
            comment : "REMOTE_DEBUG_MEM",
            name    : "REMOTE_DEBUG_MEM",
            base    : REMOTE_DEBUG_ADDR,
            len     : REMOTE_DEBUG_SIZE
        }],
        ["OCMC0_RAM", {
            comment: "OCMC0_RAM",
            name: "OCMC0_RAM",
            base: OCMC0_ADDR,
            len:  OCMC_SIZE
        }],
        ["OCMC1_RAM", {
            comment: "OCMC1_RAM",
            name: "OCMC1_RAM",
            base: OCMC1_ADDR,
            len:  OCMC_SIZE
        }],
        ["DSP_L2_RAM", {
            comment: "DSP_L2_RAM",
            name: "DSP_L2_RAM",
            base: 0x10800000,
            len:  0x00020000
        }],
    ],
    l1PMode: "32k",
    l1DMode: "32k",
    l2Mode:  "128k"
};

var addrFileGenerated = false;
if (addrFileGenerated == false)
{
    xdc.loadCapsule("genaddrinfo.xs").GenAddrFile();
    addrFileGenerated = true;
}


Please see to attached created map file

  • This is memory partitionig created by me for 2GB memory size (LInux removed from first to last 512MB region, and DSP started from REG3: 0xC0000000)

     ======== First 512 MB: =================================
     ### SR1:                         0x80000000 - 0x98000000
     ### VIDEO_M3_CODE_ADDR:          0x98000000 - 0x98800000
     ### VIDEO_M3_DATA_ADDR:          0x98800000 - 0x9a000000
     ### DSS_M3_CODE_ADDR:            0x9c000000 - 0x9c800000
     ### DSS_M3_DATA_ADDR:            0x9c800000 - 0x9e000000
     ======== Second 512 MB: =================================
     ### TILER_ADDR:                  0xa0000000 - 0xb0000000
     ### SR2_FRAME_BUFFER_ADDR:       0xb0000000 - 0xc0000000
     ========= Third 512 MB: ==================================
     ### DSP_CODE_ADDR:               0xc0000000 - 0xc1000000
     ### DSP_DATA_ADDR:               0xc1000000 - 0xdec00000
     ### SR0_ADDR:                    0xdec00000 - 0xdf800000
     ### VIDEO_M3_EXCEPTION_CTX_ADDR: 0xdf800000 - 0xdf880000
     ### VPSS_M3_EXCEPTION_CTX_ADDR:  0xdf880000 - 0xdf900000
     ### HDVPSS_DESC_ADDR:            0xdf900000 - 0xdfb00000
     ### HDVPSS_SHARED_ADDR:          0xdfb00000 - 0xdfd00000
     ### NOTIFY_SHARED_ADDR:          0xdfd00000 - 0xdff00000
     ### REMOTE_DEBUG_ADDR:           0xdff00000 - 0xe0000000
     ======== Last 512 MB: ==================================
     ### LINUX:                       0xe0000000 - 0xffffffff
     =========================================================

  • The 2G memory map you have listed will not work. There are issues apart from the linking error you are facing. For 2G memory map refer /dvr_rdk/mcfw/src_bios6/cfg/ti816x/config_2G.bld. This memory map is tested on 816x .

    You need to enable build define TI816X_2G_DDR which is currently only enabled for 816x 2G build in file

    /dvr_rdk/component.mk

    ifeq ($(DDR_MEM),DDR_MEM_2048M)
    DVR_RDK_CFLAGS += -DTI816X_2G_DDR
    endif

    Also ensure your DMM_LISA setting is correct for 2G memory map. On 814x,in some uboot configuration the DMM_LISA settings map same physical memory on 0x8xxx_xxxx to 0xAxxx_xxxx and 0xAxxx_xxxx to 0xCxxx_xxxx

  • Hello Badri,

    thanX alot for your reply. Please let me know, exist any way to run DM8148 with 2GB of physical memory (or as minimal use only 3/4 of DDR's and config for 1,5GB)? And may I ask you explain me "in deep" why my 2GB configuration file doesn't works? If 2GB tested and works on DM8168, why is porblem create 2GB configuration for DM8148. Am I understood correctly that DM814x and DM816x - both have same memory controller?

  • Marat Shchuchinsky said:
    Please let me know, exist any way to run DM8148 with 2GB of physical memory (or as minimal use only 3/4 of DDR's and config for 1,5GB)?

    As I mentioned use the 2G memory map configuration of 816x with the changes I mentioned if you want to use 2G physical memory.

    Marat Shchuchinsky said:
    If 2GB tested and works on DM8168, why is porblem create 2GB configuration for DM8148. Am I understood correctly that DM814x and DM816x - both have same memory controller?

    I don't understand your question. WHat issue are you facing using the ti816x 2G memory map on 814x ?