This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet port not able to get response for ping command (used ti8148 processor and psp version 04.01.00.07)



Hi,

           I am using ti8148 based costumed board and PSP version 04.01.00.07. When I am configuring the eth0 using the ifconfig eth0 192.168..1.xx up it is able to show the "PHY: 0:00 - Link is Up - 100/Full' status but it is unable to ping and get the response from the remote system.

I have pasted the logs of ethtool eth0 command below, so please help to resolve the issue.

root@(none):~# ethtool eth0
Settings for eth0:
        Supported ports: [ TP MII ]
        Supported link modes:   10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Half 1000baseT/Full
        Supports auto-negotiation: Yes
        Advertised link modes:  10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Half 1000baseT/Full
        Advertised pause frame use: Symmetric Receive-only
        Advertised auto-negotiation: Yes
        Speed: 100Mb/s
        Duplex: Full
        Port: MII
        PHYAD: 0
        Transceiver: external
        Auto-negotiation: on
        Current message level: 0x00000000 (0)

        Link detected: yes

I have added some debugging commands and response on the board which can be help to analysis the issue

command 1:

root@(none):~# cat /sys/class/net/eth0/carrier
1

command 2:

root@(none):~# ip link show eth0
3: eth0: <BROADCAST,MULTICAST,ALLMULTI,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast state UP qlen 1000
    link/ether 84:7e:40:e2:a4:90 brd ff:ff:ff:ff:ff:ff

command 3:

root@(none):~# ifconfig eth0
eth0      Link encap:Ethernet  HWaddr 84:7E:40:E2:A4:90
          inet addr:192.168.1.88  Bcast:192.168.1.255  Mask:255.255.255.0
          inet6 addr: fe80::867e:40ff:fee2:a490/64 Scope:Link
          UP BROADCAST RUNNING ALLMULTI MULTICAST  MTU:1500  Metric:1
          RX packets:6039 errors:0 dropped:326 overruns:0 frame:0
          TX packets:1464 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:716814 (700.0 KiB)  TX bytes:108196 (105.6 KiB)
          Interrupt:40

command 4:

root@(none):~# /etc/init.d/networking restart
Reconfiguring network interfaces... ifdown: interface lo not configured
ifdown: interface eth0 not configured

CPSW phy found : id is : 0x221622

CPSW phy found : id is : 0x221622
ADDRCONF(NETDEV_UP): eth0: link is not ready
eth0      no wireless extensions.

udhcpc (v1.13.2) started
Sending discover...
PHY: 0:00 - Link is Up - 100/Full
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Sending discover...
Sending discover...
No lease, forking to background
done.

  • Sudheer,

    Are you able to ping the host PC from u-boot?

    BR
    Pavel

  • no, I am not able to ping from u-boot.


    I have tried using the commands like

    # setenv autoload no

    # dhcp

    and pinged the host ip but it was saying it is not alive.

  • Sudheer,

    What is the mode you are using: G/MII, RMII or RGMII?

    See the below e2e thread for more info:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/358123.aspx

    BR
    Pavel

  • I am using RGMII.

    Issue in the link you mentioned was with GMII, as his interface was GMII and in evm.c file he corrected for GMII and in my case we are using RGMII only.

    I even tried to set to GMII and ping but no luck. Can you pleas once go through all the command and response which I mentioned to get any clue.

    command 1:

    TI8148_EVM#setenv autoload no

    TI8148_EVM#dhcp
    link up on port 0, speed 100, full duplex
    BOOTP broadcast 1
    BOOTP broadcast 2
    BOOTP broadcast 3
    BOOTP broadcast 4
    BOOTP broadcast 5
    BOOTP broadcast 6
    BOOTP broadcast 7
    BOOTP broadcast 8
    BOOTP broadcast 9
    BOOTP broadcast 10

    Retry count exceeded; starting again
    link up on port 0, speed 100, full duplex

    command 2:

    TI8148_EVM#ping 192.168.1.23
    link up on port 0, speed 100, full duplex
    *** ERROR: `ipaddr' not set
    ping failed; host 192.168.1.23 is not alive

  • Sudheer,

    Could you provide me full console log from the u-boot?

    What is the external ethernet PHY you are using?

    Are you aligned with the below wiki page?

    http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Ethernet_Driver_-_Adding_Custom_Ethernet_Phy

    BR
    Pavel


  •  We are using KSZ9031RNX PHY and it has the driver in Linux kernel so we have enabled the driver.

  • sudheer singh1 said:
    We are using KSZ9031RNX PHY and it has the driver in Linux kernel so we have enabled the driver.

    What about the u-boot? Can you provide me console output when you try to ping?

    BR
    Pavel

  • TI8148_EVM#setenv autoload no

    TI8148_EVM#dhcp
    link up on port 0, speed 100, full duplex
    BOOTP broadcast 1
    BOOTP broadcast 2
    BOOTP broadcast 3
    BOOTP broadcast 4
    BOOTP broadcast 5
    BOOTP broadcast 6
    BOOTP broadcast 7
    BOOTP broadcast 8
    BOOTP broadcast 9
    BOOTP broadcast 10

    Retry count exceeded; starting again
    link up on port 0, speed 100, full duplex

    command 2:

    TI8148_EVM#ping 192.168.1.23
    link up on port 0, speed 100, full duplex
    *** ERROR: `ipaddr' not set
    ping failed; host 192.168.1.23 is not alive

  • Sudheer,

    sudheer singh1 said:
    TI8148_EVM#ping 192.168.1.23
    link up on port 0, speed 100, full duplex
    *** ERROR: `ipaddr' not set
    ping failed; host 192.168.1.23 is not alive

    Can you try setting ipaddr? See how below:

    TI8148_EVM#ping 172.20.2.57
    link up on port 0, speed 100, full duplex
    *** ERROR: `ipaddr' not set
    ping failed; host 172.20.2.57 is not alive
    TI8148_EVM#setenv ipaddr 172.20.2.58
    TI8148_EVM#ping 172.20.2.57
    link up on port 0, speed 100, full duplex
    Using cpsw device
    host 172.20.2.57 is alive

    Regards,
    Pavel

  • tried but no use

    Hit any key to stop autoboot:  0
    TI8148_EVM#
    TI8148_EVM#setenv autoload no
    TI8148_EVM#setenv ipaddr 192.168.1.88
    TI8148_EVM#ping 192.168.1.23
    link up on port 0, speed 100, full duplex
    Using cpsw device
    ping failed; host 192.168.1.23 is not alive
    TI8148_EVM#ping 192.168.1.17
    link up on port 0, speed 100, full duplex
    Using cpsw device
    ping failed; host 192.168.1.17 is not alive

  • Sudheer,

    sudheer singh1 said:
    TI8148_EVM#ping 192.168.1.23

    Is 192.168.1.23 the ipaddr of your host/desktop PC?

    BR
    Pavel

  • Sudheer,

    psp 04.01.00.07 is very old software. What I recommend you is to apply all the u-boot patches related to EMAC/ethernet/net/cpsw from the ti81xx-master branch on top of your u-boot and try again.

    http://arago-project.org/git/projects/u-boot-omap3.git?p=projects/u-boot-omap3.git;a=shortlog;h=refs/heads/ti81xx-master

    BR
    Pavel

  • Sudheer,

    One more question, are you connecting your DM814x board with the host PC directly, or you have switch/hub/router between the dm814x board and the host PC?

    BR
    Pavel

  • Pavel,

                      I have tried with u-boot-04.04.00.02 psp and verified that all the patches are present in this version of psp and Ethernet response is same, not able to ping.

  • Sudheer,

    One more question, are you connecting your DM814x board with the host PC directly, or you have switch/hub/router between the dm814x board and the host PC?

    BR
    Pavel

  • Hi pavel,

                        I am using the KSZ9031RNX PHY and I have configured environment variables at u-boot level and read the register 0x01 and its value is 0x796D, in this value one bit [1] == 0 which means Jabber not detected.

    My concern is like does it should detect Jabber to make ping work.

  • Sudheer,

    sudheer singh1 said:
    My concern is like does it should detect Jabber to make ping work.

    No, I do not think you need Jabber detected to make ping work.

    sudheer singh1 said:
      I am using the KSZ9031RNX PHY

    See the below e2e thread, might be in help:

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/247923.aspx

    Best Regards,
    Pavel

  • Hi Pavel,

    I am using 14.04 on my host.

    I am using  VAR-SOM-AM33 device that is based on TI AM335x as target.

    I also try to boot the board via TFTP.

    I made the same thing that you write in the comment above:

    ping 192.168.147.136                                                    

    link up on port 0, speed 100, full duplex                                      

    link up on port 1, speed 100, full duplex                                      

    *** ERROR: `ipaddr' not set                                                    

    ping failed; host 192.168.147.136 is not alive                                  

    U-Boot# setenv ipaddr 192.168.147.136                                          

    U-Boot# ping 192.168.147.136                                                    

    link up on port 0, speed 100, full duplex                                      

    link up on port 1, speed 100, full duplex                                      

    Using cpsw device                                                              

    ping failed; host 192.168.147.136 is not alive      

     

    It seems that nothing is going out or in from the Ethernet interface.


    I am on this problem for 2 days without finding any answers.

     

    Thanks,

    Oren.

  • Hi Oren,

    oren zvuluni said:

    U-Boot# setenv ipaddr 192.168.147.136                                          

    U-Boot# ping 192.168.147.136      

    You are using the same ip addr for host (Ubuntu 14) and target (AM335x board). This is not acceptable.

    Can you provide me the output of the below command, run in on host:

    host$ ifconfig

    Can you also try with addr 192.168.147.130 instead of 192.168.147.136?

    U-Boot# setenv ipaddr 192.168.147.130                                         

    U-Boot# ping 192.168.147.136  

    Regards,
    Pavel

  • "Internal Delay" may be the cause. Please see

         e2e.ti.com/.../169742

    To disable "Internal Delay" in the u-boot

       File: uboot/ti/ti8148/evm.c

         /*program GMII_SEL register for RGMII mode */
        //__raw_writel(0x30a, GMII_SEL); // enable internal delay
        __raw_writel(0x33a, GMII_SEL); // disable internal delay

  • Pavel,

    Thanks for the responses here.

    device ifconfig output:

    root@varsomam33:~# ifconfig
    eth0      Link encap:Ethernet  HWaddr 68:9E:19:58:53:A9  
              inet addr:192.168.1.2  Bcast:192.168.1.255  Mask:255.255.255.0
              inet6 addr: fe80::6a9e:19ff:fe58:53a9/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:0 errors:0 dropped:0 overruns:0 frame:0
              TX packets:8 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:0 (0.0 B)  TX bytes:648 (648.0 B)
              Interrupt:177

    eth1      Link encap:Ethernet  HWaddr 68:9E:19:58:53:AB  
              inet addr:192.168.1.100  Bcast:192.168.1.255  Mask:255.255.255.0
              UP BROADCAST MULTICAST  MTU:1500  Metric:1
              RX packets:0 errors:0 dropped:0 overruns:0 frame:0
              TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

    lo        Link encap:Local Loopback  
              inet addr:127.0.0.1  Mask:255.0.0.0
              inet6 addr: ::1/128 Scope:Host
              UP LOOPBACK RUNNING  MTU:65536  Metric:1                              
              RX packets:127 errors:0 dropped:0 overruns:0 frame:0                  
              TX packets:127 errors:0 dropped:0 overruns:0 carrier:0                
              collisions:0 txqueuelen:0                                             
              RX bytes:208737 (203.8 KiB)  TX bytes:208737 (203.8 KiB)  

     

    Host ifconfig output:

    oren@oren-Inspiron-3542:~$ ifconfig
    eth0      Link encap:Ethernet  HWaddr 74:e6:e2:23:22:24  
              inet addr:192.168.1.1  Bcast:192.168.1.255  Mask:255.255.255.0
              inet6 addr: fe80::76e6:e2ff:fe23:2224/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:462 errors:0 dropped:0 overruns:0 frame:0
              TX packets:114 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:63286 (63.2 KB)  TX bytes:11492 (11.4 KB)

    lo        Link encap:Local Loopback  
              inet addr:127.0.0.1  Mask:255.0.0.0
              inet6 addr: ::1/128 Scope:Host
              UP LOOPBACK RUNNING  MTU:65536  Metric:1
              RX packets:3450 errors:0 dropped:0 overruns:0 frame:0
              TX packets:3450 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:0
              RX bytes:508607 (508.6 KB)  TX bytes:508607 (508.6 KB)

    wlan0     Link encap:Ethernet  HWaddr 4c:bb:58:37:48:24  
              inet addr:10.0.0.112  Bcast:10.0.0.255  Mask:255.255.255.0
              inet6 addr: fe80::4ebb:58ff:fe37:4824/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:18303 errors:0 dropped:0 overruns:0 frame:0
              TX packets:19312 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:11344575 (11.3 MB)  TX bytes:5670416 (5.6 MB)

    I tried this sequence also:

    U-Boot # setenv ipaddr 192.168.1.2
    U-Boot # setenv serverip 192.168.1.1
    U-Boot # setenv gatewayip 192.168.1.1
    U-Boot # setenv netmask 255.255.255.0

    U-Boot# ping 192.168.1.1
    link up on port 0, speed 100, full duplex
    link up on port 1, speed 100, full duplex
    Using cpsw device
    ping failed; host 192.168.1.1 is not alive

     

    The device connected directly to the PC.

    I tried to search for the GMII_SEL  that in the next reply but there is no text like that in my U-Boot suorce files.

    I think that the problem in my case is that i have two link up, The device connected to only one ETH interface and i get two link up.

    Maybe its connected to that.

     

    In DHCP mode it's the same, the device is not getting IP address from the server.

    The DHCP server is fine and working, When i am not in U-boot terminal i can configure my device to get an IP address from the DHCP server.

    Please help me.

    Thanks,

    Oren

  • Oren,

    Which AM335x eth port (eth0 or eth1) you connect to PC (eth0)?

    Which TI SDK you are using here?

    Regards,
    Pavel
  • eth0 is connected.
    How can i now what is my TI SDK? The kernel version can tell what i am using? I Downloaded the SW from arago-project site.

    How can i know what is the version?

    Thanks.

  • What is your u-boot version and from where you get it?

    The latest official TI AM335x u-boot is available at:
    software-dl.ti.com/.../index_FDS.html

    ti-processor-sdk-linux-am335x-evm-03.01.00/board-support/u-boot-2016.05

    Regards,
    Pavel
  • the u boot version is ti-u-boot-2013.01.01-amsdk-06.00.00.00.

    i got it from git.ti.com/.../ti-u-boot-2013.01.01-amsdk-06.00.00.00.

    Thanks a lot,

    oren
  • Oren,

    VAR-SOM-AM33 is designed and supported by Variscite:

    variwiki.com/index.php

    They have special forum for VAR-SOM-AM33 devices. More over they used TI SDK and aplay patches on top of the TI SDK (u-boot/kernel):

    variwiki.com/index.php
    variwiki.com/index.php

    I would suggest you to try first with TI SDK 7 and variscite patches on top. If issue remain, check with their support team.

    Regards,
    Pavel