Hi All,
We need to control some i2c slave device from VPSS M3 firmware.
We are using IPNC RDK 3.5 and I2C3 bus (instance 4)
I could able to do read write on I2C0 and I2C2 bus, but it failed read write on I2C3.
I2C interrupt number for I2C3 is given below as
"CSL_INTC_EVENTID_I2CINT3 (00u)" " I2C3 interrupt is routed through the crossbar and not used */"
Did i need to change something to make I2C3 work.?
Regards,
Manoj