This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C instance 4 support on IPNC



Hi All,

We need to control some i2c slave device from VPSS M3 firmware.

We are using IPNC RDK 3.5 and I2C3 bus (instance 4)

I could able to do read write on I2C0 and I2C2 bus, but it failed read write on I2C3.

I2C interrupt number for I2C3 is given below as

"CSL_INTC_EVENTID_I2CINT3         (00u)"  " I2C3 interrupt is routed through the crossbar and not used */"

Did i need to change something to make I2C3 work.?

Regards,

Manoj