I've been trying to determine if the dm816x series is capable of 4k (roughly 4000x2000) h264 encoding. The documentation I could find states only up to 2048x2048 but there have been a few posts on the forum that state otherwise. The dm368 series documentation does state they support it and according to what I could find it looks like it uses the same HDVICP as the dm816x so it should have the same resolution support? Our application requires 4k encode but our frame rate needs are lower, ideally 16fps but can get away with 8fps.