This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vpss load err after Watchdogtime reset



Hi:

I use dvr_rdk 3.5 platform and set 8168 watchdog time 60seconds.

After watchdog reset the system,It commit a err when run "./load_vpss.sh".It can't be load after watchdog reset system.If I reset it by hand reset switch or power off/on ,it run ok.

The print info are as follows:

Unhandled fault: external abort on non-linefetch (0x1808) at 0xf9020000
Internal error: : 1808 [#1]
last sysfs file: /sys/kernel/uevent_seqnum
Modules linked in: syslink
CPU: 0 Not tainted (2.6.37 #13)
PC is at DM8168DUCATIMMU_enable+0x60/0xa0 [syslink]
LR is at DM8168DUCATIMMU_enable+0x28/0xa0 [syslink]
pc : [<bf0171dc>] lr : [<bf0171a4>] psr: 00000013
sp : cb7acff0 ip : d4e01000 fp : cb7ad004
r10: 00000000 r9 : cb7ac000 r8 : bf0af4e4
r7 : bf07c98c r6 : d4dfe000 r5 : 00000000 r4 : d4dfe000
r3 : 00010000 r2 : f9020000 r1 : 00060000 r0 : bf0613d3
Flags: nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: 8c260019 DAC: 00000015
Process fw_load.out (pid: 968, stack limit = 0xcb7ac2e8)
Stack: (0xcb7acff0 to 0xcb7ae000)

Are there someone meet this similar phenomenon ? How to solve it if i want watchdog time reset and run to well?

  • Hi,

    Watchdog reset is a warm reset and hence it doesn't reset all the modules. This is the reason for the above hang/ errors.

    Please try this uboot patch :

    diff --git a/arch/arm/cpu/arm_cortexa8/start.S b/arch/arm/cpu/arm_cortexa8/start.S
    index 423b01b..260dbc7 100644
    --- a/arch/arm/cpu/arm_cortexa8/start.S
    +++ b/arch/arm/cpu/arm_cortexa8/start.S
    @@ -95,6 +95,11 @@ FIQ_STACK_START:
     	.word 0x0badc0de
     #endif
     
    +
    +#define PRM_DEVICE_RSTTST 0x481800A8
    +prm_device_rsttst:
    + .word PRM_DEVICE_RSTTST
    +
     /*
      * the actual reset code
      */
    @@ -107,6 +112,15 @@ reset:
     	bic	r0, r0, #0x1f
     	orr	r0, r0, #0xd3
     	msr	cpsr,r0
    +  /*Force cold reset if a 
    +   warm reset is detected*/
    +  ldr r0, prm_device_rsttst
    +  ldr r1, [r0]
    +  str r1, [r0]
    +  cmp r1, #2
    +  beq reset_cpu
    +  cmp r1, #8
    +  beq reset_cpu
     
     #if (CONFIG_OMAP34XX)
     	/* Copy vectors to mask ROM indirect addr */
    diff --git a/board/ti/ti8168_dvr/dvr.c b/board/ti/ti8168_dvr/dvr.c
    index d6ab5f1..38733f2 100644
    --- a/board/ti/ti8168_dvr/dvr.c
    +++ b/board/ti/ti8168_dvr/dvr.c
    @@ -1246,6 +1246,8 @@ void s_init(u32 in_ddr)
     #ifdef CONFIG_TI816X_VOLT_SCALE
     	voltage_scale_init();
     #endif
    +
    +  udelay(100);
     }
     
     /* optionally do something like blinking LED */
    
    . This patch is for ti816x UD works dvr and has uboot changes to detect a warm reset and force cold reset. 

    Please refer to thread http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/276202/1026048.aspx#1026048 for more details on the above changes.

    Regards,

    Reshma