This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816X dvrrdk350 encoder capability?



Hi:

    DM816X DVRRDK encoder link support encoder:

    5 chanel 1080P25 8M bitrates?

   or  5 channel 720P25 8M bitrates?

    now I met when set encoder bitrates 8M,it will lost some frame

   My input is 5 channel 1080P30 or 5 channel 720P60 input

  • Hi ,

    What speed grade chip are you using and what is the speed setting ??

    And what kind of encoder,   h264 hp, mp ,bp , etc...     What is the maximum bitrate you ever tested that no frame is lost ?

    Also make sure the skipframe is disabled.

    Their are many other causes that might affect the performance of encoder.

    BR,

    Eason