Hi:
DM816X DVRRDK encoder link support encoder:
5 chanel 1080P25 8M bitrates?
or 5 channel 720P25 8M bitrates?
now I met when set encoder bitrates 8M,it will lost some frame
My input is 5 channel 1080P30 or 5 channel 720P60 input
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
DM816X DVRRDK encoder link support encoder:
5 chanel 1080P25 8M bitrates?
or 5 channel 720P25 8M bitrates?
now I met when set encoder bitrates 8M,it will lost some frame
My input is 5 channel 1080P30 or 5 channel 720P60 input
Hi ,
What speed grade chip are you using and what is the speed setting ??
And what kind of encoder, h264 hp, mp ,bp , etc... What is the maximum bitrate you ever tested that no frame is lost ?
Also make sure the skipframe is disabled.
Their are many other causes that might affect the performance of encoder.
BR,
Eason