This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 GPMC Performance and Throughput



Hi all,

I'm using a Gumstix Overo 3530 kit (256MB RAM / 256MB NAND) with a LAN9221 Ethernet and intend to connect a customised FPGA to the GPMC bus on synchronous R/W access. I'm running  Linux v2.6.39 kernel

I need help and points in estimating the performance and throughput of the GPMC in such configuration.

Discussion 1:

I read from the TRM that the GPMC has a maximum speed of 100MHz if and only if the L3 Clock is at 100MHz.

But from my investigation, the L3 clock is running at 166MHz instead and this limits the GPMC clock to 83MHz.

I've read from past discussion that the throughput of the ethernet bus is not efficient and is it because of this 83MHz limitation?

Discussion 2:

In order to use the maximum 100MHz for my FPGA, can the L3 clock be switch on-the-fly without affect other devices that uses the GPMC bus? i.e. the ethernet chip.

My guess is that we cannot do such on-the-fly switching of the L3 clock.  Please enlighten me if this can be done and stable.

Discussion 3:

How do I model my setup and mathematically estimate the utilization of the GPMC bus?

Assuming the maximum transfer size of 1 R/W cycle for the devices are,

  • LAN9221 - Maximum MTU (1500 bytes)
  • RAM - 1 page
  • ROM - 1 page
  • FPGA - 125kbytes

Discussion 4:

With multiple devices on the GPMC bus, how does the OMAP does its scheduling when there is a contention to use the GPMC resources?

i.e. Between Ethernet and FPGA

 

Many thanks in adv.

Please pardon my newbies questions as I'm just learning OMAP3+Linux.

 

Regards,

James

 

  • James.Ang said:

    Discussion 1:

    I read from the TRM that the GPMC has a maximum speed of 100MHz if and only if the L3 Clock is at 100MHz.

    But from my investigation, the L3 clock is running at 166MHz instead and this limits the GPMC clock to 83MHz.

    I've read from past discussion that the throughput of the ethernet bus is not efficient and is it because of this 83MHz limitation?

    That's part of it.  The external device makes a difference too.  I recall hearing of performance differences due to things such as the size of the FIFO integrated into the external Ethernet device.

     

    James.Ang said:

    Discussion 2:

    In order to use the maximum 100MHz for my FPGA, can the L3 clock be switch on-the-fly without affect other devices that uses the GPMC bus? i.e. the ethernet chip.

    My guess is that we cannot do such on-the-fly switching of the L3 clock.  Please enlighten me if this can be done and stable.

    Not easily anyways... The L3 interconnect frequency is ALSO the frequency for the LPDDR, so by changing the L3 frequency you would also be changing your LPDDR clock speed.  I imagine you would need to put the LPDDR in self-refresh, change the L3 clock speed, modify the SDRC timings, and then take the SDRC out of self-refresh.  All this code would need to run from internal memory so it would be a royal pain to set it all up.  In short I think I would steer clear!

     

    James.Ang said:

    Discussion 3:

    How do I model my setup and mathematically estimate the utilization of the GPMC bus?

    Assuming the maximum transfer size of 1 R/W cycle for the devices are,

    • LAN9221 - Maximum MTU (1500 bytes)
    • RAM - 1 page
    • ROM - 1 page
    • FPGA - 125kbytes

    Can't you stick a logic analyzer on there and measure it?  Does your FPGA support chip-scope?

     

    James.Ang said:

    Discussion 4:

    With multiple devices on the GPMC bus, how does the OMAP does its scheduling when there is a contention to use the GPMC resources?

    i.e. Between Ethernet and FPGA

    The GPMC is considered a "target" on the L3 interconnect.  The arbitration would happen at the L3 interconnect level.  See the L3 Interconnect chapter of the TRM for starters.

  • Brad Griffis said:

    Discussion 1:

    I read from the TRM that the GPMC has a maximum speed of 100MHz if and only if the L3 Clock is at 100MHz.

    But from my investigation, the L3 clock is running at 166MHz instead and this limits the GPMC clock to 83MHz.

    I've read from past discussion that the throughput of the ethernet bus is not efficient and is it because of this 83MHz limitation?

    That's part of it.  The external device makes a difference too.  I recall hearing of performance differences due to things such as the size of the FIFO integrated into the external Ethernet device.

    [/quote]

    Hmm.. I agreed on that point.

    If all else the same, the GPMC clock will be the differentiating factor for throughput between the devices.

     

    Brad Griffis said:

    Discussion 2:

    In order to use the maximum 100MHz for my FPGA, can the L3 clock be switch on-the-fly without affect other devices that uses the GPMC bus? i.e. the ethernet chip.

    My guess is that we cannot do such on-the-fly switching of the L3 clock.  Please enlighten me if this can be done and stable.

    Not easily anyways... The L3 interconnect frequency is ALSO the frequency for the LPDDR, so by changing the L3 frequency you would also be changing your LPDDR clock speed.  I imagine you would need to put the LPDDR in self-refresh, change the L3 clock speed, modify the SDRC timings, and then take the SDRC out of self-refresh.  All this code would need to run from internal memory so it would be a royal pain to set it all up.  In short I think I would steer clear!

    [/quote]

    I agreed too.. Too much of a task to handle.

     

    Brad Griffis said:

    Discussion 3:

    How do I model my setup and mathematically estimate the utilization of the GPMC bus?

    Assuming the maximum transfer size of 1 R/W cycle for the devices are,

    • LAN9221 - Maximum MTU (1500 bytes)
    • RAM - 1 page
    • ROM - 1 page
    • FPGA - 125kbytes

    Can't you stick a logic analyzer on there and measure it?  Does your FPGA support chip-scope?

    [/quote]

    Err.. I don't have such equipment on hand and I just need a theoretically calculation model to estimate it to estimate the latency between transfer.

     

    Brad Griffis said:

    Discussion 4:

    With multiple devices on the GPMC bus, how does the OMAP does its scheduling when there is a contention to use the GPMC resources?

    i.e. Between Ethernet and FPGA

    The GPMC is considered a "target" on the L3 interconnect.  The arbitration would happen at the L3 interconnect level.  See the L3 Interconnect chapter of the TRM for starters.

    [/quote]

    Noted. On that.

    Is there a configuration in the Linux Kernel which can be used to change the priority of servicing the hardware request. i.e. putting the FPGA at and higher priority than the Ethernet.

     

    Thanks in adv.

    James.

  • James.Ang said:

    Err.. I don't have such equipment on hand and I just need a theoretically calculation model to estimate it to estimate the latency between transfer.

    I guess the next best thing would be to use the internal device timers to measure the time for doing various tasks in isolation.  I don't expect mathematical models to be a very productive use of time, nor do I expect you would be very accurate.  The systems are so complicated at this point you really need to just measure stuff.

     

    James.Ang said:
    Is there a configuration in the Linux Kernel which can be used to change the priority of servicing the hardware request. i.e. putting the FPGA at and higher priority than the Ethernet.

    You might post a separate question in the Linux forum.  I don't believe there is anything.