Other Parts Discussed in Thread: TMS320C6713B
We are having an in issue with a TMS320C6713B. Most of the time, our code is executing with no issues; we power up using Host Boot mode and all is well. However, sometimes on power up we program in Host Boot mode (and read back the checksum over the HPI bus and all appears to be well), but the processor appears to never start.
We have checked the state of all HD pins when the reset is released. They all appear OK, including the 'Do Not Oppose' pins in the datasheet.
We have checked the nTRST, EMU0/1 and they are the correct state on power up. The CLK0 pin is also correct.
We have checked the length of the rest pulse. It quite sufficient and appears stable (no extra glitches). We have verified that the reset pulse occurs after the power supplies are stable.
We have altered the power supply sequencing so that the 3.3V doesn't even start coming up until the core voltage is stable. No change.
What are some other things we should be checking? It is very odd in that once the processor does not start on a power up, subsequent pulses of the reset line do nothing.... it is some state on a particular power up that is permanent until we cycle the power again.
Thanks in advance for any support!