This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSK6713 THS1206 TLV5630

Other Parts Discussed in Thread: TLV5630, THS1206

Hi,

i'm using a DSK6713 and the TI-ADC THS1206 and the TI-DAC TLV5630.

The TLV5630 is using the MCBSP0 and the THS1206 is on the Modular THS1206 EVM.

When I use the Data Converter Support in CCS3.3 i'm able to use only one of the peripherals.

My question: Is it possible to use the ADC and DAC on the DSK6713?

Is there any example-code?

  • Robin Lerche,

    Robin: said:
    My question: Is it possible to use the ADC and DAC on the DSK6713?
    Is there any example-code? 

    Kindly have a look at the below wiki for DSK. It gives the software download link.
    http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5
    After download the DSK6713 software package, you can find the BSL and test code.
    This board have the audio codec(tlv320aic23). It has the in-built ADC and DAC for Audio.
    Refer the 6713_dsk_techref.pdf and tlv320aic23.pdf

    And also refer the product folder as mentioned the below link,
    http://www.ti.com/tool/tmdsdsk6713 

    http://www.ti.com/tool/ths1206m-evm
    http://www.ti.com/product/TLV5630

    Queries on ADC/DAC are best handled by Precision Data Converters Forum.

    The below thread may help for your understanding
    http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/2927.aspx

  • Hey Pubesh,

    thank you for your fast answer. I'm sorry, but I described my problem not good enough.

    I'm trying to configure the McBSP0 on the DSK6713. I want to connect a SPI-Device at first, but it doesn't work.

    I tested the McBSP1-Channel too and nothing happend.

    Maybe you can help me now better.

    Best regards

    Robin

  • Robin,

    Yes, you can do McBSP as SPI master or slave.

    DSK6713:
    McBSP0 is used as the unidirectional control channel.
    It should be programmed to send a 16-bit control word to the AIC23 in SPI format.

    McBSP1 is used as the bi-directional data channel.
    All audio data flows through the data channel.
    Many data formats are supported based on the three variables of sample width, clock signal source and serial data format.

    Please have a look at the McBSP file.

    /*
     * Copyright (C) 2003 Texas Instruments Incorporated
     * All Rights Reserved
     */
    /*
     *---------main_mcbsp1.c---------
     *
     * mcbsp1 Example configures the serial port for digital loopback mode.
     * We then use the CPU to write/read from the port. In loopback mode, we 
     * should read back the same value as written, which is checked for in a loop
     */
    #include <stdio.h>
    #include <csl.h>
    #include <csl_mcbsp.h>
    
    /* create a config structure for digital loopback mode */
    static MCBSP_Config ConfigLoopback = {
      
      /* Serial Port Control Register (SPCR) */
      MCBSP_SPCR_RMK(        
      
        MCBSP_SPCR_FREE_YES, /* Serial clock free running mode(FREE)
                                  MCBSP_SPCR_FREE_NO - During emulation halt,SOFT bit
                                       determines operation of McBSP.
                                  MCBSP_SPCR_FREE_YES - During emulation halt, serial 
                                       clocks continue to run.                     */                                                     
        
        MCBSP_SPCR_SOFT_YES, /* Serial clock emulation mode(SOFT)
                                  MCBSP_SPCR_SOFT_NO -  In conjunction with FREE = 0, 
                                       serial port clock stops immediately during 
                                       emulation halt,thus aborting any transmissions.          
                                  MCBSP_SPCR_SOFT_YES - In conjunction with FREE = 0, 
                                       during emulation halt, serial port clock stops
                                       after completion of current transmission.   */
                                  
        MCBSP_SPCR_FRST_YES, /* Frame sync generator reset(FRST)
                                  MCBSP_SPCR_FRST_YES /MCBSP_SPCR_FRST_0 - Frame sync 
                                       generation logic is reset.
                                  MCBSP_SPCR_FRST_NO /MCBSP_SPCR_FRST_1  - Frame sync
                                       signal is generated after eight CLKG clocks. */ 
                   
        MCBSP_SPCR_GRST_YES, /* Sample rate generator reset(GRST)
                                 MCBSP_SPCR_GRST_YES /MCBSP_SPCR_GRST_0  - Reset    
                                 MCBSP_SPCR_GRST_NO /MCBSP_SPCR_GRST_1 -Out of reset*/   
        
        MCBSP_SPCR_XINTM_XRDY,/* Transmit interrupt mode(XINTM) 
                                 MCBSP_SPCR_XINTM_XRDY - XINT driven by XRDY    
                                 MCBSP_SPCR_XINTM_EOS  - XINT generated by 
                                       end-of-subframe in multichannel operation    
                                 MCBSP_SPCR_XINTM_FRM  - XINT generated by a new frame
                                       synchronization    
                                 MCBSP_SPCR_XINTM_XSYNCERR - XINT generated by XSYNCERR
                                                                                    */
        MCBSP_SPCR_XSYNCERR_NO,/* Transmit synchronization error  
                                 MCBSP_SPCR_XSYNCERR_NO /MCBSP_SPCR_XSYNCERR_0  - No 
                                       frame synchronization error
                                 MCBSP_SPCR_XSYNCERR_YES /MCBSP_SPCR_XSYNCERR_1 - Frame 
                                       synchronization error detected by McBSP       */
        
        MCBSP_SPCR_XRST_YES, /* Transmitter reset(XRST). This resets or enables 
                                transmitter.
                                 MCBSP_SPCR_XRST_YES /MCBSP_SPCR_XRST_0  - Serial port 
                                       transmitter is disabled and is in reset state.
                                 MCBSP_SPCR_XRST_NO /MCBSP_SPCR_XRST_1   - Serial port 
                                       transmitter is enabled.                       */  
        
        MCBSP_SPCR_DLB_ON,   /* Digital loopback(DLB) mode 
                                 MCBSP_SPCR_DLB_OFF   - DLB Disabled 
                                 MCBSP_SPCR_DLB_ON    - DLB Enabled                  */ 
        
        MCBSP_SPCR_RJUST_RZF,/*Receive data sign-extension and justification mode(RJUST)
                                 MCBSP_SPCR_RJUST_RZF - Right-justify and zero-fill 
                                       MSBs in DRR.  
                                 MCBSP_SPCR_RJUST_RSE - Right-justify and sign-extend
                                       MSBs in DRR.
                                 MCBSP_SPCR_RJUST_LZF - Left-justify and zero-fill 
                                       LSBs in DRR.                                  */
        
        MCBSP_SPCR_CLKSTP_DISABLE,/* Clock stop(CLKSTP) mode
                                 MCBSP_SPCR_CLKSTP_DISABLE - Disabled. Normal 
                                      clocking enabled for non-SPI mode.               
                                 MCBSP_SPCR_CLKSTP_NODELAY -Clock starts without delay.                               
                                 MCBSP_SPCR_CLKSTP_DELAY   - Clock starts with delay.*/
        
        MCBSP_SPCR_DXENA_OFF,/* DX Enabler(DXENA) -Extra delay for DX turn-on time.
                                 Only first bit of data is delayed.
                                 MCBSP_SPCR_DXENA_OFF - DX enabler is off.       
                                 MCBSP_SPCR_DXENA_ON  - DX enabler is on.            */ 
        
        MCBSP_SPCR_RINTM_RRDY,/* Receive interrupt(RINT) mode
                                 MCBSP_SPCR_RINTM_RRDY - RINT driven by RRDY    
                                 MCBSP_SPCR_RINTM_EOS  - RINT generated by 
                                      end-of-subframe in multichannel operation
                                 MCBSP_SPCR_RINTM_FRM  - RINT generated by a new frame
                                      synchronization    
                                 MCBSP_SPCR_RINTM_RSYNCERR -RINT generated by RSYNCERR*/
       
        MCBSP_SPCR_RSYNCERR_NO,/* Receive synchronization error(RSYNCERR)
                                 MCBSP_SPCR_RSYNCERR_NO /MCBSP_SPCR_RSYNCERR_0 - No
                                      frame synchronization error
                                 MCBSP_SPCR_RSYNCERR_YES /MCBSP_SPCR_RSYNCERR_1 - Frame
                                      synchronization error detected by McBSP         */ 
                                   
        MCBSP_SPCR_RRST_YES /* Receiver reset(RRST). This resets or enables
                               receiver.       
                                 MCBSP_SPCR_RRST_YES /MCBSP_SPCR_RRST_0 - Serial 
                                     port receiver is disabled and is in reset state. 
                                 MCBSP_SPCR_RRST_NO  /MCBSP_SPCR_RRST_1 - Serial
                                      port receiver is enabled.                    */
        
      ),
        
      /*  Receive Control Register (RCR) */
      MCBSP_RCR_RMK(  
      
        MCBSP_RCR_RPHASE_SINGLE, /* Receive phases 
                                 MCBSP_RCR_RPHASE_SINGLE - Single phase frame                          
                                 MCBSP_RCR_RPHASE_DUAL   - Dual phase frame        */
                                  
        MCBSP_RCR_RFRLEN2_OF(0), /* Receive frame length in phase 2(RFRLEN2) 
                                  000 0000b: 1 word per phase     
                                  000 0001b: 2 words per phase
                                  . . . . . . . . . . . . 
                                  111 1111b: 128 words per phase                   */
        
        MCBSP_RCR_RWDLEN2_8BIT,/* Receive element length in phase 2(RWDLEN2)  
                                 MCBSP_RCR_RWDLEN2_8BIT  -  8  bits   
                                 MCBSP_RCR_RWDLEN2_12BIT -  12 bits
                                 MCBSP_RCR_RWDLEN2_16BIT -  16 bits
                                 MCBSP_RCR_RWDLEN2_20BIT -  20 bits
                                 MCBSP_RCR_RWDLEN2_24BIT -  24 bits
                                 MCBSP_RCR_RWDLEN2_32BIT -  32 bits                */
                                 
        MCBSP_RCR_RCOMPAND_MSB,/* Receive companding mode (RCOMPAND)  
                                 MCBSP_RCR_RCOMPAND_MSB  - No companding.Data 
                                      transfer starts with MSB first.    
                                 MCBSP_RCR_RCOMPAND_8BITLSB - No companding, 
                                      8-bit data. Transfer starts with LSB first. 
                                      Applicable to 8-bit data or 32-bit data in 
                                      data reversal mode. 
                                 MCBSP_RCR_RCOMPAND_ULAW -  Compand using m-law for
                                      receive data. Applicable to 8-bit data only   
                                 MCBSP_RCR_RCOMPAND_ALAW - Compand using A-law for 
                                      receive data. Applicable to 8-bit data only  */  
         
        MCBSP_RCR_RFIG_YES, /* Receive frame ignore(RFIG)
                                 MCBSP_RCR_RFIG_NO  - Unexpected receive frame
                                      synchronization pulses restart the transfer.  
                                 MCBSP_RCR_RFIG_YES - Unexpected receive frame
                                      synchronization pulses are ignored.          */
                                      
        MCBSP_RCR_RDATDLY_0BIT,/* Receive data delay(RDATDLY)
                                 MCBSP_RCR_RDATDLY_0BIT - 0 bit data delay 
                                 MCBSP_RCR_RDATDLY_1BIT - 1 bit data delay
                                 MCBSP_RCR_RDATDLY_2BIT - 2 bit data delay         */
        
        MCBSP_RCR_RFRLEN1_OF(0), /* Receive frame length in phase 1(RFRLEN1)
                                 000 0000b: 1 word per phase 
                                 000 0001b: 2 words per phase
                                 . . . . . . . . . . . . 
                                 111 1111b: 128 words per phase                    */ 
                                 
        MCBSP_RCR_RWDLEN1_32BIT,/* Receive element length in phase 1(RWDLEN1)
        
                                 MCBSP_RCR_RWDLEN1_8BIT  -  8 bits
                                 MCBSP_RCR_RWDLEN1_12BIT - 12 bits 
                                 MCBSP_RCR_RWDLEN1_16BIT - 16 bits 
                                 MCBSP_RCR_RWDLEN1_20BIT - 20 bits 
                                 MCBSP_RCR_RWDLEN1_24BIT - 24 bits
                                 MCBSP_RCR_RWDLEN1_32BIT - 32 bits                 */
        
        MCBSP_RCR_RWDREVRS_DISABLE/* Receive 32-bit bit reversal feature.(RWDREVRS)
                                 MCBSP_RCR_RWDREVRS_DISABLE -32 bit reversal disabled
                                 MCBSP_RCR_RWDREVRS_ENABLE  -32 bit reversal enabled. 
                                      32-bit data is received LSB first.        
                                      RWDLEN should be set for 32-bit operation.
                                      RCOMPAND should be set to 01b else operation
                                      is undefined.                                */
      ),
    
      /* Transmit Control Register (XCR) */
      MCBSP_XCR_RMK(            
        
        MCBSP_XCR_XPHASE_SINGLE,/* Transmit phases
                                 MCBSP_XCR_XPHASE_SINGLE - Single phase frame
                                 MCBSP_XCR_XPHASE_DUAL   - Dual phase frame       */
        
        MCBSP_XCR_XFRLEN2_OF(0),/* Transmit frame length in phase 2(XFRLEN2) 
                                 000 0000b: 1 word per phase   
                                 000 0001b: 2 words per phase  
                                 . . . . . . . . . . . .       
                                 111 1111b: 128 words per phase                   */
                                 
        MCBSP_XCR_XWDLEN2_8BIT, /*  Transmit element length in phase 2
                                 MCBSP_XCR_XWDLEN2_8BIT    -  8  bits                   
                                 MCBSP_XCR_XWDLEN2_12BIT   -  12 bits                   
                                 MCBSP_XCR_XWDLEN2_16BIT   -  16 bits                   
                                 MCBSP_XCR_XWDLEN2_20BIT   -  20 bits                   
                                 MCBSP_XCR_XWDLEN2_24BIT   -  24 bits                   
                                 MCBSP_XCR_XWDLEN2_32BIT   -  32 bits             */
      
        MCBSP_XCR_XCOMPAND_MSB, /* Transmit companding mode(XCOMPAND)
                                 MCBSP_XCR_XCOMPAND_MSB      - No companding. Data 
                                      transfer starts with MSB first.
                                 MCBSP_XCR_XCOMPAND_8BITLSB  - No companding, 8-bit
                                       data. Transfer starts with LSB first. 
                                       Applicable to 8-bit data,or 32-bit data in 
                                       data reversal mode.    
                                 MCBSP_XCR_XCOMPAND_ULAW     - Compand using m-law
                                       for receive data.Applicable to 8-bit data only.
                                 MCBSP_XCR_XCOMPAND_ALAW  - Compand using A-law for
                                       receive data.Applicable to 8-bit data only. */
        
        MCBSP_XCR_XFIG_YES, /* Transmit frame ignore(XFIG)
                                 MCBSP_XCR_XFIG_NO  - Unexpected transmit frame
                                       synchronization pulses restart the transfer.
                                 MCBSP_XCR_XFIG_YES - Unexpected transmit frame 
                                       synchronization pulses are ignored.         */
        
        MCBSP_XCR_XDATDLY_0BIT, /*  Transmit data delay(XDATDLY)
                                 MCBSP_XCR_XDATDLY_0BIT   - 0 bit data delay             
                                 MCBSP_XCR_XDATDLY_1BIT   - 1 bit data delay            
                                 MCBSP_XCR_XDATDLY_2BIT   - 2 bit data delay       */ 
        
        MCBSP_XCR_XFRLEN1_OF(0), /* Transmit frame length in phase 1(XFRLEN1)
                                 000 0000b: 1 word per phase 
                                 000 0001b: 2 words per phase
                                 . . . . . . . . . . . . 
                                 111 1111b: 128 words per phase                    */ 
    
        MCBSP_XCR_XWDLEN1_32BIT, /* Transmit element length in phase 1(XWDLEN1)
                                 MCBSP_XCR_XWDLEN1_8BIT  -   8 bits                     
                                 MCBSP_XCR_XWDLEN1_12BIT -  12 bits                     
                                 MCBSP_XCR_XWDLEN1_16BIT -  16 bits                     
                                 MCBSP_XCR_XWDLEN1_20BIT -  20 bits                      
                                 MCBSP_XCR_XWDLEN1_24BIT -  24 bits                     
                                 MCBSP_XCR_XWDLEN1_32BIT -  32 bits                */  
    
       MCBSP_XCR_XWDREVRS_DISABLE /* Transmit 32-bit bit reversal feature
                                  MCBSP_XCR_XWDREVRS_DISABLE - 32-bit reversal
                                       disabled.
                                  MCBSP_XCR_XWDREVRS_ENABLE  - 32-bit reversal 
                                       enabled. 32-bit data is transmitted LSB first.
                                       XWDLEN should be set for 32-bit operation.
                                       XCOMPAND should be set to 01b; else operation
                                       is undefined.                               */  
       
      ),
      
      /*serial port sample rate generator register(SRGR) */
      MCBSP_SRGR_RMK( 
      
        MCBSP_SRGR_GSYNC_FREE,/* Sample rate generator clock synchronization(GSYNC).
                                 MCBSP_SRGR_GSYNC_FREE - The sample rate generator 
                                      clock CLKG) is free running.
                                 MCBSP_SRGR_GSYNC_SYNC - (CLKG) is running but is 
                                       resynchronized, and the frame sync signal
                                       (FSG)is generated only after the receive
                                       frame synchronization signal(FSR)is detected.
                                       Also,the frame period (FPER) is a don�t care 
                                       because the period is dictated by the external
                                       frame sync pulse.                            */
                                 
        MCBSP_SRGR_CLKSP_RISING,/* CLKS polarity clock edge select(CLKSP)
                                  MCBSP_SRGR_CLKSP_RISING  - The rising edge of CLKS 
                                       generates CLKG and FSG.
                                  MCBSP_SRGR_CLKSP_FALLING - The falling edge of CLKS
                                       generates CLKG and FSG.                      */
        MCBSP_SRGR_CLKSM_INTERNAL,/* MCBSP sample rate generator clock mode(CLKSM)
                                  MCBSP_SRGR_CLKSM_CLKS   - The sample rate generator
                                       clock is derived from CLKS. 
                                  MCBSP_SRGR_CLKSM_INTERNAL - (Default value) The
                                       sample rate generator clock is derived from
                                       the internal clock source.                   */
    
        MCBSP_SRGR_FSGM_DXR2XSR,/*Sample rate generator transmit frame synchronization
                                   mode.(FSGM)
                                  MCBSP_SRGR_FSGM_DXR2XSR  - The transmit frame sync
                                       signal (FSX) is generated on every DXR to XSR
                                       copy.                                                        
                                  MCBSP_SRGR_FSGM_FSG      - The transmit frame sync
                                       signal is driven by the sample rate generator
                                       frame sync signal, FSG.                      */
       
        MCBSP_SRGR_FPER_OF(63),/* Frame period(FPER)
                                  Valid values: 0 to 4095                           */    
        
        MCBSP_SRGR_FWID_OF(31),/* Frame width(FWID)
                                  Valid values: 0 to 255                            */
                                  
        MCBSP_SRGR_CLKGDV_OF(15)/* Sample rate generator clock divider(CLKGDV)
                                  Valid values: 0 to 255                            */
        
      ),
      
      MCBSP_MCR_DEFAULT, /* Using default value of MCR register */
      MCBSP_RCER_DEFAULT,/* Using default value of RCER register */
      MCBSP_XCER_DEFAULT,/* Using default value of XCER register */
      
      /* serial port pin control register(PCR) */
      MCBSP_PCR_RMK(   
      
        MCBSP_PCR_XIOEN_SP, /* Transmitter in general-purpose I/O mode - only when 
                               XRST = 0 in SPCR - (XIOEN)
                               MCBSP_PCR_XIOEN_SP    -  CLKS pin is not a general 
                                    purpose input. DX pin is not a general purpose
                                    output.FSX and CLKX are not general-purpose I/Os.
                               MCBSP_PCR_XIOEN_GPIO  -  CLKS pin is a general-purpose
                                    input. DX pin is a general-purpose output. 
                                    FSX and CLKX are general-purpose I/Os. These
                                    serial port pins do not perform serial port
                                    operation.                                     */
        MCBSP_PCR_RIOEN_SP, /* Receiver in general-purpose I/O mode - only when 
                               RRST = 0 in SPCR -(RIOEN)
                               MCBSP_PCR_RIOEN_SP    - DR and CLKS pins are not 
                                    general-purpose inputs. FSR and CLKR are not 
                                    general-purpose I/Os and perform serial port 
                                    operation.
                               MCBSP_PCR_RIOEN_GPIO  - DR and CLKS pins are 
                                    general-purpose inputs. FSR and CLKR are 
                                    general-purpose I/Os. These serial port pins do
                                    not perform serial port operation.            */  
        MCBSP_PCR_FSXM_INTERNAL, /* Transmit frame synchronization mode(FSXM)
                                 MCBSP_PCR_FSXM_EXTERNAL - Frame synchronization 
                                      signal is provided by an external source. FSX
                                      is an input pin. 
                                 MCBSP_PCR_FSXM_INTERNAL - Frame synchronization 
                                      generation is determined by the sample rate 
                                      generator frame synchronization mode bit FSGM
                                      in the SRGR.                                */
        
        MCBSP_PCR_FSRM_EXTERNAL, /* Receive frame synchronization mode (FSRM)
                                 MCBSP_PCR_FSRM_EXTERNAL  - Frame synchronization 
                                      signals are generated by an external device.
                                      FSR is an input pin.                              
                                 MCBSP_PCR_FSRM_INTERNAL  - Frame synchronization 
                                      signals are generated internally by the sample
                                      rate generator. FSR is an output pin except 
                                      when GSYNC = 1 in SRGR.                     */     
        
        MCBSP_PCR_CLKXM_OUTPUT, /* Transmitter clock mode (CLKXM)
                                 MCBSP_PCR_CLKXM_INPUT    -  Transmitter clock is 
                                      driven by an external clock with CLKX as an
                                      input pin.
                                 MCBSP_PCR_CLKXM_OUTPUT   - CLKX is an output pin
                                       and is driven by the internal sample rate
                                       generator.
                                 
                                 During SPI mode :
                                 MCBSP_PCR_CLKXM_INPUT    -  McBSP is a slave and 
                                      (CLKX) is driven by the SPI master in the 
                                       system. CLKR is internally driven by CLKX.
                                 MCBSP_PCR_CLKXM_OUTPUT   - McBSP is a master and 
                                      generates the transmitter clock (CLKX) to
                                      drive its receiver clock (CLKR) and the shift
                                      clock of the SPI-compliant slaves in the 
                                      system.                                     */  
        MCBSP_PCR_CLKRM_INPUT, /* Receiver clock mode (CLKRM)
                                  
                                  Case 1: Digital loopback mode not set in SPCR
                                  
                                  MCBSP_PCR_CLKRM_INPUT - Receive clock (CLKR) is 
                                       an input driven by an external clock.
                                       
                                  MCBSP_PCR_CLKRM_OUTPUT -  CLKR is an output pin 
                                       and is driven by the sample rate generator.
                                  
                                  Case 2: Digital loopback mode set  in SPCR
                                  
                                  MCBSP_PCR_CLKRM_INPUT - Receive clock  is driven
                                       by the transmit clock (CLKX), which is based
                                       on the CLKXM bit in PCR. CLKR is in high 
                                       impedance.
                                  MCBSP_PCR_CLKRM_INPUT - CLKR is an output pin and
                                       is driven by the transmit clock. The transmit
                                       clock is derived from CLKXM bit in the PCR.*/
        
        
        MCBSP_PCR_CLKSSTAT_0, /*  CLKS pin status(CLKSSTAT)
                                  MCBSP_PCR_CLKSSTAT_0  
                                  MCBSP_PCR_CLKSSTAT_1                            */
        
        MCBSP_PCR_DXSTAT_0,   /*  DX pin status(DXSTAT)
                                  MCBSP_PCR_DXSTAT_0
                                  MCBSP_PCR_DXSTAT_1                              */
        
        MCBSP_PCR_FSXP_ACTIVEHIGH, /* Transmit frame synchronization polarity(FSXP)
                                  MCBSP_PCR_FSXP_ACTIVEHIGH - Frame synchronization
                                           pulse FSX is active high
                                  MCBSP_PCR_FSXP_ACTIVELOW  - Frame synchronization
                                       pulse FSX is active low                    */
        MCBSP_PCR_FSRP_ACTIVEHIGH, /* Receive frame synchronization polarity(FSRP)
                                  MCBSP_PCR_FSRP_ACTIVEHIGH - Frame synchronization
                                       pulse FSR is active high
                                  MCBSP_PCR_FSRP_ACTIVELOW  - Frame synchronization 
                                       pulse FSR is active low                    */
        MCBSP_PCR_CLKXP_RISING, /* Transmit clock polarity(CLKXP)
                                  MCBSP_PCR_CLKXP_RISING - Transmit data driven on 
                                       rising edge of CLKX
                                  MCBSP_PCR_CLKXP_FALLING - Transmit data driven on
                                        falling edge of CLKX                      */
        MCBSP_PCR_CLKRP_FALLING /* Receive clock polarity(CLKRP)
                                  MCBSP_PCR_CLKRP_FALLING - Receive data sampled on
                                       falling edge of CLKR
                                  MCBSP_PCR_CLKRP_RISING - Receive data sampled on
                                        rising edge of CLKR                       */
      )
    }; 
    
    /* ---------------------------------------------------------------------------*/  
    void main() {
    
      MCBSP_Handle hMcbsp;  
      volatile Uint32 x,y;
      int success = 1;
      
      /* Initialize the chip support library, must when using CSL */
      CSL_init();
    
      /* Let's open up serial port 1 */
      hMcbsp = MCBSP_open(MCBSP_DEV1, MCBSP_OPEN_RESET);
      
      /* We'll set it up for digital loopback, 32bit mode. We have   */
      /* to setup the sample rate generator to allow self clocking.  */
      MCBSP_config(hMcbsp,&ConfigLoopback);
    
      /* Now that the port is setup, let's enable it in steps. */
      MCBSP_start(hMcbsp,MCBSP_RCV_START | MCBSP_XMIT_START |
       					 MCBSP_SRGR_START| MCBSP_SRGR_FRAMESYNC,
       			  MCBSP_SRGR_DEFAULT_DELAY);
         
    
      /* Now we'll loop for a while writing values out to the port */
      /* then reading them back in. This should take a few seconds.*/
      for (y=0; y<0x00080000; y++) {  
      
        /* wait until the transmitter is ready for a sample then write to it */
        while (!MCBSP_xrdy(hMcbsp));                       
        MCBSP_write(hMcbsp,y);
      
        /* now wait until the value is received then read it */
        while (!MCBSP_rrdy(hMcbsp));           
        x = MCBSP_read(hMcbsp);
        
        /* check to make sure they match */
        if (x != y) {
          success = 0;
          printf("\nTEST FAILED");
          break;
        } 
      }
      
      /* All done now, close the port. */
      MCBSP_close(hMcbsp); 
      if(success)  
        printf("\nTEST PASSED\n");
    }
    

  • The THS1206 EVM does not and cannot use the McBSP.  It has a parallel interface.  Note that the 5-6K Interface Board requires you to choose whether you're using each of its two "slots" for serial or parallel EVM.