This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Am335x SPI Master DO signal too low



Hi,

How do you configure the PINS correctly ? I heard that you have to put RXACTIVE=1 for the SCLK signal ( which doesn't make sense ) .

My problem is the output from the spi master, the signal doesn't get above 1.12V And I don't know why ? I have only a pull up resistor between the am335X SPI DO and the max3107 SPI DI .

my config :

0x164 0x24 /* (C18) eCAP0_in_PWM0_out.spi1_sclk ok*/
0x168 0x0C /* (E18) uart0_ctsn.spi1_d0 */
0x16c 0x14 /* (E17) uart0_rtsn.spi1_d1 */
0x170 0x11 /* (E15) uart0_rxd.spi1_cs0 */
0x174 0x11 /* (E16) uart0_txd.spi1_cs1 */

Any Idea ?