Other Parts Discussed in Thread: CC2650, BLE-STACK
First, I set VIMS mode disable like below.
VIMSModeSet( VIMS_BASE, VIMS_MODE_DISABLED );
// Wait for disabling to be complete
while ( VIMSModeGet( VIMS_BASE ) != VIMS_MODE_DISABLED );
but I don't know what is the address of RAM start ,RAM size etc..
i changed like below,but it doesn't work.
if ( isdefinedsymbol(CC2650) ) { define symbol RAM_SIZE = 0x00007000; // 28K//0x00005000; // 20K define symbol FLASH_SIZE = 0x00020000; // 128K define symbol ROM_SIZE = 0x0001C000; // 115K } //////////////////////////////////////////////////////////////////////////////// // Default else { define symbol RAM_SIZE = 0x00004000; // 16K define symbol FLASH_SIZE = 0x00020000; // 128K define symbol ROM_SIZE = 0x00018000; // 96K }
//////////////////////////////////////////////////////////////////////////////// // Memory Definitions ////////////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////////// // RAM //
define symbol RAM_START = 0x01FFFE000;//x20000000
if ( isdefinedsymbol(CC2650) ) { if ( isdefinedsymbol(ICALL_RAM0_ADDR) ) { define symbol RAM_END = (ICALL_RAM0_ADDR-1); } else // default { define symbol RAM_END = 0x20006A00; } } else // CC2650 PG1 { if ( isdefinedsymbol(ICALL_RAM0_ADDR) ) { define symbol RAM_END = (ICALL_RAM0_ADDR-1); } else // default { define symbol RAM_END = 0x200029FF; } }