Dear TI experts,
We have such an app: After the two-way camera images are processed by the Viss node, they are split by the Split node. One image is given to the LDC node 0 for processing, and the other image is given to the LDC nodes 1, 2, and 3 for processing. The four images output by the LDC are then cropped and scaled by the Mosaic node, and finally displayed. The delays of the four LDC nodes are shown in the figure. May I ask if the delay of the LDC hardware is the sum of the delays of the four nodes or the maximum value of the delays of the four nodes? Currently, the input and output dimensions of the four LDC nodes are both 1920x1536. Can the LDC hardware meet the 60fps requirement under such conditions? What is the upper limit of the computing power of the LDC hardware?
Best,