Hello,
I'm currently exploring the custom reel option via the Texas Instruments API and have a couple of questions that I hope some of you might be able to help with.
-
I noticed that on the TI web store, the custom reel option is only displayed when adding a certain quantity of parts to the cart, typically 55 pieces or more. However, when using the inventory and pricing API (https://api-portal.ti.com/store-inventory-pricing-api), it doesn't specify the minimum quantity at which the custom reel option is available. If we were to order less than 55 pieces of the same part via the API and set the customReelIndicator to true, would the order still be accepted? Is it possible to purchase the custom reel option regardless of the quantity of the part we are ordering?
-
I've also heard that it might be necessary to set up a module to enable the CustomReel option. However, I'm not entirely sure about this. Can anyone confirm whether this module setup is indeed required? If so, could you provide some guidance on how to go about this setup?
Any insights would be greatly appreciated. Thank you in advance.
Best,