This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-API: TI-TXT-005 - Pricing could not be determined

Part Number: TI-API

Tool/software:

Hey,

I created a test order on the backlog route: transact.ti.com/.../test

The data I submitted was this josn structure:

{"order":
    {
     "endCustomerCompanyName": "XX",
     "checkoutProfileId": "XX",
     "customerPurchaseOrderNumber": 97,
     "lineItems": [{
            "customerLineItemNumber": 1,
            "tiPartNumber": "INA240A2PW",
            "customerPartNumber": "34053130",
            "quoteNumber": "",
            "customerAnticipatedUnitPrice": "1.799",
            "customerCurrencyCode": "USD",
            "schedules": [{"requestedQuantity": "450", "requestedDeliveryDate": "2025-07-10"}]
      }]
   }
}
I recieve the message with the code TI-TXT-005: "Pricing could not be determined".
Why is that so? When will the price be available?
Thank you for your help,
Linus

**Attention** This is a public forum