Part Number: SN75115
The DS shows the NS package dimensions, but the visual example is a 14-pin version showing pin-pitch is 1.27mm, and the "length" dimension (A) is 10.50mm.
I am a little confused and just want to confirm, but on the same page, it lists the 16-pin device as having the same "A" length of 10.50mm.
For other pin counts, the A length is different...so what I want to know is if the pin-pitch is 1.27mm for both 14-pin and 16-pin options, and the package "A" dimension really is 10.50mm for both.
If so, then I guess there is some "extra mold material padding" for the 14-pin option?