Part Number: TUSB564
Other Parts Discussed in Thread: TUSB1064
We use TUSB564(TUSB564IRNQT) as DP sink device re-driver. It have a performance issue. The output frame can not higher than 40frame @4K.
Our schematic is the picture "schematic.jpg".
The chip mark is the picture "device marking.jpg".
In test mode, input/output waveform is the picture "input_output.jpg". 
Below is the question:
1.We read the register from the TUSB564 address 0x00~0x07. value is the following:
00=54 ;
01=55 ;
02=53 ;
03=42 ;
04=31 ;
05=30 ;
06=36 ;
07=34 ;
The ASCII is "TUSB1064",Does it means the assembling chip is TUSB1064 ?
2.Could the TUSB1064 replace TUSB564?
3.Through TUSB564 the signal wave become worse,How to change the configuration of TUSB564 to reslove the problem?