Part Number: DS90UB948-Q1
Hi ,TI:
Hello, we need to design a large-screen machine that meets the ISO26262-B standard. Do the following functions of DS90UB948 support?
1. Does the chip support FPD-LINK data verification? After verifying the data error, it will be returned to the master through the differential link?
2. Does the chip support LVDS data verification, and the data error is returned to the master through the differential link?
3. Does the chip support I2C anomaly detection? When an I2C anomaly is detected, it will be fed back to the master through a differential link?
4. Is it possible to read back the CRC check result on the screen through the LVDS differential link?