This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4551-Q1: Interesting fields missing from Interrupts register 0x0820

Part Number: TCAN4551-Q1
Other Parts Discussed in Thread: TCAN4550

I notice in the demonstration software in the structure TCAN4x5x_Device_Interrupts, there are a number of diagnostic flags that can highlight CAN hardware problems, such as:

uint8_t CBF : 1;

uint8_t CANBUSBAT : 1;
uint8_t CANBUSGND : 1;
uint8_t CANBUSOPEN : 1;
uint8_t CANLGND : 1;
uint8_t CANHBAT : 1;
uint8_t CANHCANL : 1;
uint8_t CANBUSTERMOPEN : 1;

However, these are all reserved in the data sheet.

Are they no longer supported?

Are there any guides on what flags are available to perform bus error diagnostics and recovery?

Thanks.