Other Parts Discussed in Thread: ESDS314, ESDS312
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
I need a TVS to protect HDMI signals. The surge that we are trying to suppress is similar to waveform 4 in the MIL-STD-461 G (please refer to the waveform below). 4.6 uS risetime to 100V and then decays to @ 50% in 69uS.
Is a double exponential with risetime of 6.4 uS and fall to 50% in 69 uS. The Vmax. = 100 V. and max. current of 333A. It is a part of the conducted susceptibility 117 (for Lightning), not just for regular ESD
The circuit I need to protect has a absolute max. voltage of 3.6V. The TVS needs to be capable of sustaining @ 1.15 k-Watts for 69 uS.

Regards,
Danilo