Other Parts Discussed in Thread: SN75ALS193, DS34C86T, AM26C32, AM26LV32
I have really struggling searching through all the devices.
I am in need of a Line Receiver (quad, or 2x dual) to handle receiving a total of 4x differential inputs, and output a single-ended H/L signal for each differential input.
(Basically 4x differential input line receivers)
The use-case will have 120Ω termination resistors. TI has a lot of devices that state "failsafe when outputs are open; Output = HIGH" but they are just 100k or 300k pullup/pulldown resistors on the input lines.
So when 120Ω termination is used, the VID is around 1~2mV for 5V supply voltage. But the devices usually needs VID >200mV in order to set the output HIGH.
The goal is to find a device that supports differential inputs where VID can be up to ±5V, and termination resistors can be used, while the device still allows for an open-condition at the inputs to result in the output being either HIGH or LOW.
It looks like one way to do this is to add 330Ω-or-so pullup/pulldown resistors to A and B, but the goal is not to have these external resistors on the lines.
Ignoring package size for now, are there any quad/dual devices that have failsafe outputs when input is "open", that still work when 120Ω termination resistors are used?
EDIT:
I was reviewing slyt514 and snla031 and it looks like the standard use-case is to have the low-Ω Fail-Safe biasing resistors on the Master/Host side (Tx), so the Rx side only needs the termination resistor.
I am understanding devices like SN75ALS193 have integrated 300kΩ biasing resistors for failsafe, which work when there is no termination resistor between A/B. But when there is termination, the resistors are too large, and we don't achieve >200mV needed to ensure output is HIGH. Correct?
Is there any literature on using failsafe biasing for both Tx (Host) and Rx (Device)?
Regards,
Darren
Darren