Part Number: TCAN1145-Q1
Dear team,
After powering up, my customer write 0x10=0x07 to our device to enter normal mode, but our device has no response. I am not sure whether we need to make more operation to enter normal mode. We read 0x00 register, SDO output two bytes, one is 0x50=0xA0, and another is 0x00=0x54. The 0x00 register value is correct, but the 0x50 seems incorrect. We need to clear these interrupt, then we can enter normal mode, right?
In addition, we also test the SCK rise time, in the datasheet, the max value is 40ns, but the actual SCK rise time is ~45ns. Why does our device has this limit? If SCK rise time is larger than 40ns, is there any bad impact?
Thanks & Regards,
Sherry