Part Number: SN65LVDS31-EP
Hi Team,
In one of our customer's application they need to provide information concerning the fault tolerance of SN65LVDS31-EP. In cases of failure of the LVDS receiver (end-device), 3.6V will be directly applied to the differential outputs Y and Z pin. The reference post mentions that the SN65LVDS31-EP output can withstand VCC+0.5V, would this still be applicable even if the applied voltage (due to the receiver fault) to the output is 3.6V (VCC max)?
Thanks in advance!
Kind Regards,
Jejomar