Other Parts Discussed in Thread: TUSB1064, , TUSB564
hi,
My customer use TUSB1064 for type C alternate mode.
for display port, they only need 5.4G. But the distance between TUSB1064 and scalar is more than 32cm.
They are afraid that the signal quality for DP.
Can they put SN75DP130 after TUSB1064 to enhance the signal quality?
By the way, they also use 10G Usb3 hub.
BR,
frank