Part Number: SN65HVD37
Hi Team
My customer have 2 questions about SN65HVD37.
Please kindly help with these. It will be appreciate.
1. Datasheet says VOH(min) is 2.4V on Pin 2(Receiver) when IOH=-8mA.
Customer wants to connect Pin 2 to another device, which VIH(min) is 2.64V. So here's the problem.
IOH was actually not -8mA but only several uA in their application, is there any graph showing IOH for y-axis and VOH for x-axis?
Customer wants to conclude that, "when IOH is several uA, VOH is above 2.64V", so they can use SN65HVD37 in this case.
2. What is output impedance(ohm) for Y and Z pin and how can customer calculate it?
There is no VOL, VOH for Pin Y and Z in datasheet.
Please advise us.
Thanks.
Regards,
Jo