Part Number: TUSB542
Hi team,
My customer is evaluating the TUSB542 on trial board. The customer would like to have the answer to the questions below urgently. Could you please help with the questions below?
1. The d/s describes the Xtalk as -45dB(typ). How much will be the maximum?
2. There are two systems, RX_CON2 vs TX_CON2 and RX_CON1 vs TX_CON1. Are there any differences in crosstalk between the two systems? If so, which one is worse?
3. The power supply voltage is 1.8V. Could you tell me the recommended bypass capacitance value?
4. GND is connected with 6 pieces of VIA diameter 0.1 mm. Is this considered sufficient?
Regards,
Yamaguchi