Part Number: TPS7A43
Other Parts Discussed in Thread: TPS7B82-Q1, TPS7B63-Q1, TPS7B70-Q1, TPS7B4253-Q1, TPS7B7701-Q1
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "bd4269efj-ce2" ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS7A43
Other Parts Discussed in Thread: TPS7B82-Q1, TPS7B63-Q1, TPS7B70-Q1, TPS7B4253-Q1, TPS7B7701-Q1
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "bd4269efj-ce2" ?
Please allow us one additional business day for us to look into this for you and we will get back to you soon.
Hello Kygo,
There are multiple parts that can be used here. Please let me know if you have any questions.
Regards,
Prakash L
| BD4269 | TPS7B82-Q1 | TPS7B63-Q1 | TPS7B70-Q1 | TPS7B4253-Q1 | TPS7B7701-Q1 | |
| AEC Q100 | YES | YES | YES | YES | YES | YES |
| Output Options | Fixed Output | Fixed Output | Fixed Output | Fixed Output | Adjustable Output, Tracking Output | Adjustable Output |
| Iout (Max) (A) | 0.3 | 0.3 | 0.3 | 0.3 | 0.3 | 0.3 |
| Vin (Max) (V) | 45 | 40 | 40 | 40 | 40 | 40 |
| Vin (Min) (V) | 5.5 | 3 | 4 | 4 | 4 | 4 |
| Vout (Max) (V) | 5 | 5 | 5 | 5 | 40 | 20 |
| Vout (Min) (V) | 5 | 3.3 | 3.3 | 3.3 | 1.5 | 1.5 |
| Fixed Output Options (V) | 5 | 3.3, 5 | 3.3, 5 | 5, 3.3 | - | - |
| Enable | NO | YES | YES | YES | YES | YES |
| Power Good | NO | NO | YES | YES | NO | YES |
| Output Capacitor Type | Ceramic | Ceramic | Ceramic, Non-Ceramic | Ceramic, Non-Ceramic | Ceramic, Non-Ceramic | Ceramic, Non-Ceramic |
| PSRR @ 100KHz (dB) | - | 25 | 55 | 40 | 60 | 60 |
| Noise (uVrms) | - | 450 | - | - | - | - |
| Accuracy (%) | 3 | 2 | 2 | 2 | - | 2 |
| Vdo (Typ) (mV) | 250 | 400 | 300 | 300 | 350 | 350 |
| Iq (Typ) (mA) | 0.07 | 0.003 | 0.019 | 0.019 | 0.04 | 0.6 |
| Thermal Resistance θJA (°C/W) | 130 | 59 | 40 | 39.7 | 45 | 40 |
| Min Package Area (mm2) | 19.159 | 4 | 32 | 32 | 19.071 | 32 |
| Package Type | SOIC, SOPowerPAD | HVSSOP, TO-252, WSON | HTSSOP | HTSSOP | HTSSOP, SO PowerPAD | HTSSOP |