Other Parts Discussed in Thread: TPD1E10B06-Q1, TVS0500
Hello,
I am a beginner in the field of ESD protections and need the support of TI to choose the right ESD protection component and design the circuit.
Setup:
An external signal comes as an input to a GPIO pin of the uC (F280049C). This signal is not a high-speed signal. And there is a resistor divider from the connector pin to reduce the levels to 3.3V and then it is connected to the GPIO pin of the uC.
Application:
Automotive EVs (the external signal comes from the wiring harness)
Requirement:
ESD protection for this GPIO pin. Now, I have gone through the ESD essential series from TI and I understand various IEC 61000 standards. But I am unable to design the ESD protection circuitry. Hence, I have posted down several questions below.
1. I understand I need to qualify for IEC 61000-4-2 level 4. But I am not sure which level do I need to qualify for IEC 61000-4-5 surge protection. I could not find relevant information for it. With your experience, can you let me know what would be the level required for IEC 61000-4-5?
2. I am planning to use ESD351. But it has only a 6A rating for an 8/20us surge. So, my plan was to use a series resistor between the conn pin and ESD351. This should reduce the current going into the ESD531 during higher surges. Is this a good idea?
a. Since, the resistor will see the higher voltage across it, what kind of resistor do I need to choose?
b. ESD351 has a clamping voltage of 6.5V at 16A. Will this 6.5V damage the GPIO pin or do I need to also add a series resistor between ESD351 and GPIO pin?
So, will this arrangement work:
Conn Pin -> Resistor -> ESD351 -> Resistor -> GPIO pin
Or is there a better arrangement that is generally used?
3. Another arrangement is to use a series resistor and then a Schottky protection diode to the supply rails. Which is a better protection design for this specific application - the TVS one or the Schottky one?
4. Will the Schottky idea qualify for IEC standards? What are your thoughts on that?
It would be nice if you can answer these questions in detail for better understanding. Thanks for your time.