This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9539: The status of GPIO before power on

Part Number: TCA9539


Hi Team,

According to the DS, the GPIO config at power on is config as input. The customer wants to know the config before power on. I guess it should be Hi-z mode, please kindly help to double confirm.

The reason why the customer asking is that they are using these GPIO ports to output.
They’re afraid the floating and impact the design function if the port setup to output before configure.

However, it should be okay, if the port config is input before power on. Thank you.

Best regards,

Mike