Part Number: SN65DP159
I would like to output 3840x1080 @ 60p using SN65DP159RGZ. Is it possible?
The data sheet says that it is compatible with HDMI 2.0a, so I think it can be used without problems in terms of bandwidth.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DP159
I would like to output 3840x1080 @ 60p using SN65DP159RGZ. Is it possible?
The data sheet says that it is compatible with HDMI 2.0a, so I think it can be used without problems in terms of bandwidth.
Hi,
3840x1080 is the active pixel count, what is the total pixel count? And what is the required bits/pixel, 24bpp?
To calculate the total bandwidth
Total bandwidth = Total horizonal pixel * Total vertical pixel * bits/pixel * 60 * 10/8
HDMI2.0 bandwidth is 6G/lane, total bandwidth is 18G. If the total bandwidth of the resolution is less than 18G, then the DP159 can support it.
Thanks
David