Other Parts Discussed in Thread: DP83869EVM, DP83869
hello,
we want to design DP83869evm to send data but not to receive data using fiber 1000BaseX. DP83869evm have work on the media converter mode and have disabled atuo-negotiation by strap option. if fiber rx is not connected with fiber cable, we see the LED_2 is off and FX_STS[2] is link down. so if sfp rx is not connected with fiber cable , how to operate in 1000BASE-X through the register settings for 1000base-x link up? In the “DP83869 1000Base-X Link Detection”, if Serdes Synchronization status bit (0x4F[8]) is set,the phy may achieve a successful 1000Base-X link-up, so how can i have SerDes synchronization?
regards,
jane