Part Number: SN65LVDS22
Hi Team,
Is it possible to DC Bias without AC coupling on an LVDS line, something like fig 3 but without the capacitors? Not sure if this could cause damage to the device driver?
Use case is SN65LVDS22 (3.3V) paired with an FPGA (2.5V) with the DC bias powered from the 2.5V. AC coupling is not an option in the application but the customer would like the additional protection DC biasing offers.
Thanks and best regards,
Dan