Part Number: SN65DP159
Hi team,
Can you have a look at the following customer question?
The control pins are specified with max. 30µA (High Level Input current). This would be a pull-up of Min 110kOhm => 3.3V / 30µA
However, you specify 65kOhm in the application example. Which value/specification is correct or in which range may the resistor value lie?


Thank you,
Franz