Part Number: TUSB1046EVM
Other Parts Discussed in Thread: TUSB1064
I'm prototyping a USB Type-C charging hub that allows DP Alt-mode traffic to pass through.
Although the product features lists that the EVM can be operated in DFP or UFP mode (controlled via I2C), the user guide only specifies using the type-c as UFP. Moreover, the board only has type-B and type-C receptacles, so the connectivity is unclear (or nonconformant?) if the type-C is the DFP.
My assumption was that I could use two TUSB1046EVMs, back-to-back, in the following configuration:
1. TUSB1046EVM in DFP mode, connected to host - receiving USB SS + DP (2 lanes) from host, acting as PD source towards host.
Sending USB-SS signal over the USB-B (?) receptacle, through a USB3 hub, towards the 2nd EVM.
Sending DP signal over a DisplayPort cable, towards the 2nd EVM.
2. TUSB1046EVM in UFP mode, connected to display - receiving USB SS (from type-B receptacle) and DP (from DP receptacle).
Any idea how the DFP mode operates on the TUSB1046EVM?
Alternatively, I could use the following configuration:
1. TIDA01243 connected to host
Sending USB-SS signal over the USB-A receptacle towards the 2nd EVM
Sending DP signal over a mini-DP<->DisplayPort cable, towards the TUSB1046EVM.
2. TUSB1046EVM in UFP mode, connected to display - receiving USB SS (from type-B receptacle) and DP (from DP receptacle).
Can you please comment on whether this setup is expected to work for high-speed (2 lane, 4K@60fps) DP traffic without additional components.