Part Number: TCAN1044V-Q1
Hello CAN team,
TI has CAN IC with Vio (V version) and without Vio (Non-V version) such as TCAN1042(V)-Q1 and TCAN1044(V)-Q1.
In this simplified internal block diagram, there are pullup to "VCC or VIO" on the TXD, RXD, STB pins.
For the CAN without Vio (Non-V version) this pull-up is connected to VCC, and for the CAN with Vio (V version) this pullup is connected to Vio, correct?
For the CAN with Vio (V version), No voltage will show up on the TXD, RXD STB pin when it is after supplying VCC 5V but before supplying Vio (3.3V for example), correct?

Regards,
Hirata