Part Number: DS90UB921-Q1
Other Parts Discussed in Thread: DS90UB940-Q1
I have several questions regarding TI's SerDes video interface. It looks like the DS90UB921-Q1 (serializer) and DS90UB940-Q1 gives a solution to start with. My questions are:
- Is there a path/roadmap to 4K (or better) video transmission?
- Schematics for the dev boards list Rosenberger connectors D4S20D-40ML5-Y and D4S20D-40ML5-Z, which I cannot find an exact match for on their site, and the link in TI documentation is dead. Rosenberger lists D4S20D-40MA5-_ as a valid part number. I understand the last character is the key, but there is one more character difference. I see LAF-101-1000-Y-Z as potentially the cable to mate the two connectors/dev boards together. Is that correct? Is a cable like this to connect a serializer and deserializer available through TI, or we do we need to go through Rosenberger or other supplier?
- Is there any recommended standard cabling or input/output video devices to connect to the dev boards listed above? I do have some devices but the terminal connectors/cables and pinout on your boards and mine are not necessarily standard for the Parallel and MIPI interfaces so I'm wondering the best way to connect them. Would individual jumper wires work - I wouldn't think so.
Thanks for the support.
-Nick