Part Number: SN65HVD234
Hi
Our system using SN65HVD234D for CAN communication .
But we have some isseus CAN communication.
This is our TEST result
1) System Side SN65HVD234D ( Termination Resister 120ohm ) ==== > CAN Device ( Termination Resister 120ohm )
=> This is CAN Communication is OK
2) System Side SN65HVD234D ( Termination Resister 120ohm ) ==> CAN Device 1 ( Termination Resister 120ohm ) =>> CAN Device 2 ( Termination Resister 120ohm )
=> Yes , Our System Connect two CAN device with 2 each Termiantion Resister ( 120ohm x 2)
【Question】
Sorry...I did not know detail for CAN interface spec.
Is it correct for our this CAN Connect system ( MCU: 120ohm , CAN Deivice 1 :120ohm , CAN Device 2 :120ohm) ??
Regard
March Jasper ( In Japan )