Hi Experts,
Can 933 support RGB888, RGB565 and BT1120? If yes, how to calculate the maximum pclk it can support respectively? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Can 933 support RGB888, RGB565 and BT1120? If yes, how to calculate the maximum pclk it can support respectively? Thank you.
Hello Arie,
This would be more of a question for the sensor vendors. Do you have a DVP-type sensor with up to 12 data pins and a clock that would be able to transmit such data types? If so, then please consult with the imager vendor for how they would pack those data types into the 12bit parallel interface. i.e. 1 pixel per two clock cycles, 1 pixel per three clock cycles, etc.
Best Regards,
Casey